Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Aluminum Rim

Aluminum Rim
Sales Price: 31.99 SGD
Review Rating: 4.67
6 Customer Reviews
5 star 4
4 star 2
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
My bicycle
From Japan
On 2016-05-07 19:35:39
In order to exchange to the air hub of Bridgestone subnard Nakano Iron Works, it was troublesome to remove the spoke from the rim that was originally attached, so I bought this new rim and watched it with a spoke. It is completely uncomfortable with the bicycle of Bridgestone, we have been riding for about a year, but we can use anything without problems. I am trying to replace other bicycles, so I am currently considering repeating.
This review is about item#08499898.
For the utilization of the hub on hand
From Japan
On 2014-08-18 22:14:50
Because it was made by ARAYA, I purchased it without hesitation. There was a hub for loading, so we assembled it in combination. I decimated the spokes considerably and assembled, but the swing fits in moderation and it is complete. There used to be a flat tire due to burr fragments on other rims before, so we cleaned deburrs by themselves. It will be helpful if you increase the kind of spokes. It is not related to this product, but I am happy that BB can handle it.
This review is about item#36795333.
For replacement when the rim deformation breakage
From Japan
On 2014-03-14 14:40:33
I used it for electric-assisted bicycle but it can be used well.
This review is about item#36795333.
Rim exchange of damaged wheels
From Japan
On 2012-06-04 11:40:07
Naturally it can be used normally. The price is similar to that of internet selling stores, but it is very advantageous that shipping costs are not applied. Anyway, I'd like you to line up a cooler rim (aero etc).
This review is about item#36795342.
Bicycle rim exchange
From Japan
On 2011-12-29 17:14:03
Since "27 × 1 1/4 use" can also be used for 27 × 1 3/8, I used the LP - 60 for a normal masking 27 inch 13/8. There is a burr in the spoke hole etc and it is a product which has not been deburred, but since the nipple is made of iron etc., even if there is burr of aluminum it can be assembled without worry so we could assemble without problems. When buying a rim, a large shipping cost is applied and there are many cases where the shipping fee is high, but it is good that the shipping fee became free so it is free shipping fee of 3000 yen or more.
This review is about item#36795315.
Repair of an accident bicycle, but only when repair is possible.
From Japan
On 2011-09-08 06:39:15
Although it is a new home made in China, quality is no problem. No matter how much I searched, there was no sale of the rim alone. I was honestly surprised to be monotaro. It was saved.
This review is about item#36795333.
Customer Who Viewed This Item Also Viewed
Spoke Thread Chaser
Freewheel Remover
Spoke CP
Pasela, PaselaW / O
Unit Rear Hub
Fork, With Bracket
Spoke SB Stainless
Aluminum Rim Set
Transmission Back Stick Set
Stainless Rim
Internal Assembly
ATB Rear Wheel
Aluminum Front Wheel
Bicycle Rear Wheels
Stainless Rim Set