Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Straight Bit, Guide Bearing

Straight Bit, Guide Bearing
Sales Price: 36.99 SGD
Review Rating: 4.25
4 Customer Reviews
5 star 2
4 star 1
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 4 of 4 Reviews
Trimmer type board work
5
From Japan
On 2017-06-22 10:01:10
Sharpness is also good and easy to use If there is a blade diameter φ 12 mm, Ureshii It is still better if the shaft length is a little more
This review is about item#37027907.
Woodworking
5
From Japan
On 2016-05-24 15:33:26
Sharpness is also useful.
Guitar processing
3
From Japan
On 2014-06-19 09:59:44
It was well broken and easy to use. Just when purchasing it is necessary to open another page from the catalog as details on the size are not written. I wish I could write the size just like any other product
This review is about item#37027907.
Wood processing
4
From Japan
On 2013-12-18 09:07:16
I am satisfied with the price compared with other shops and the feeling I used. However, the delivered product was different in image length and blade length. This time it happened that it worked well because it worked well, so it is evaluated as "satisfied". Even with this guide roller type, it would be nice if there was a cheap edition product.
This review is about item#37027907.
1
Customer Who Viewed This Item Also Viewed
Carbide straight bit
Trimmer router bit
Straight with guide bearing
Router Bit
Straight Router Bit
polishing machine for joints
Machine for joints long
W Bearing Corner Bit
Machine for joints DX
Router Bit
Easy Nick Bit
Solid Carbide Straight Bit