Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Combination Padlock,Change Lock

Combination Padlock,Change Lock
Sales Price: 12.99 SGD
Review Rating: 4.00
3 Customer Reviews
5 star 2
4 star 0
3 star 0
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 3 of 3 Reviews
To the key lock of the door
5
From Japan
On 2017-06-19 08:42:39
I built a small barn and used it as a key for that door. I am thinking that I am worried because the operation is also easy and it is a manufacturer item.
This review is about item#37135472.
Lock of large stainless post
5
From Japan
On 2017-01-11 08:31:42
The brass body has a high-class feeling, but the price may be cheap. I bought it for locking a large stainless post, but the size and the legibility of figures were exactly right. Because stainless steel has only a large 40 mm size hook part, it is even better if you can choose stainless steel even for small size. When changing the key number, turning the hook 180 degrees to the opposite side in the unlocked state, changing it to the desired number while pushing it further, and then releasing the hook was easy with completion. The point of noting does not turn if you try to rotate the dial while pulling the main body during the unlocking operation, so you have to match the numbers with the hook pushed into the main body. Since I use dial lock for the first time, I do not know if it is such a specification in general, but if the dial happens to turn while pulling it happens that the numbers match happen, it opens easily, so it is not a problem in operation.
This review is about item#37135472.
Warehouse entrance
2
From Japan
On 2013-12-25 15:53:14
I set it as instructed but I can not set it did not work. I am in trouble because I do not understand figures, but I want you to tell me if I know how to release it.
This review is about item#37135874.
1
Customer Who Viewed This Item Also Viewed
Cable Lock
Dial Combination Lock
Combination Padlock
YALe dial padlock
Square Combination Padlock
4-Digit Combination Lock
Combination Padlock
Combination Padlock Key
Push Button Padlock
4 Dial Padlock