Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of LA Coupling HI-LA type

LA Coupling HI-LA type
Sales Price: 12.99 SGD
Review Rating: 5.00
5 Customer Reviews
5 star 5
4 star 0
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
I used it when CUP can not be struck at the time of water leakage.
5
From Japan
On 2017-09-16 10:11:55
Without this product, leakage repair could not be done, so this product is pretty handy. We will also purchase.
This review is about item#36953183.
When replacing the water pipe
5
From Japan
On 2017-07-01 17:07:40
Since the water pipe leaked in the water pipe at the start of the water pipe for 40 years and it was inside the wall, repair of the start-up was impossible, the connection part with the PVC pipe could not be relaxed, so the water pipe of the start-up was thunder Cut it off and use this coupling there is good workability There is no omission Construction is completed in a blink of an eye. I thought that it would be good if only a little more thickness was thin.
This review is about item#36953183.
Stop water pipe
5
From Japan
On 2017-01-16 17:38:08
It was saved because it was a small place where work using dice can not be done.
This review is about item#36953183.
Joint of rotten steel pipe and PVC pipe
5
From Japan
On 2016-05-29 16:59:32
It can be installed easily without threading. It is convenient ♪
I used it to join the corroded piping.
5
From Japan
On 2015-06-05 09:07:53
It does not require a short nipple and withstands pressures up to 10 K, so it is convenient for replacing piping with air or liquid.
This review is about item#36953192.
1