Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Round Can

Round Can
Sales Price: 3.99 SGD
Review Rating: 3.50
4 Customer Reviews
5 star 1
4 star 1
3 star 1
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 4 of 4 Reviews
Experiment
5
From Japan
On 2016-12-12 07:49:30
Especially it seems to be usable without problems. After that, although it is durable, it is only for static electricity, so I am concerned only with rusting due to humidity.
This review is about item#37319597.
Used as a motif of drawing
2
From Japan
On 2015-06-23 13:13:58
When checking all of the 55 delivered items, there are three deformations (deflections) that can be corrected by hand, some are deformed as if a force was applied by something like a radio pliers There were inconveniences at the rate of two pieces of things, a little less than 10% of the whole thing. Both of them are openings of the can, the one that can be modified is possibly at the time of transportation, and the one that can not be modified is considered to be a problem at the time of manufacture.
This review is about item#37319597.
Used as a motif of drawing
3
From Japan
On 2015-06-09 16:45:44
I'm sorry, I do not think there is any problem with the product itself, but when unpacking one that you sent about 50 orders in two boxes, one can placed at the end "snakes" The whole form was not "cylinder". I put it in my hand and corrected it slowly, but I picked it up, but I could not have done this.
This review is about item#37319597.
As part of the homemade rain shelter
4
From Japan
On 2013-11-07 13:43:41
Is no problem. I'm glad I bought it. However, because it was unfamiliar with the purchase method, if you want to stock 20 items with 18 stocks, you need to buy with 18 pieces first, then 2 separate orders in the backordered state I knew it later, we had to change the situation that 20 orders were put together for the operator at a later date and it was awaiting backorder. I felt it difficult if I did not get used to it.
This review is about item#37319554.
1
Customer Who Viewed This Item Also Viewed
Aluminum Screw Cap Can
Tamtam Cans
Tall Beaker
Round Can Lid
AG18-8 Kitchen Pot
Handless Glass
Stainless Steel Canister
Can
Stain universal can
Stainless steel cup
Stainless steel container
18-8 round cruet (knob-free)
18-8 Bain Marie pot
18-8 seasoning cans stocker
Plain Cans
Round Tin Cans
Oil Pail