Buy more than* S$200* and get FREE SHIPPING
Due to the maintenance, we will close our website on June/19 9:00-10:00 and June/23 0:00-0:30 JST. All customers cannot shop on our website during the time. Thank you.

Customer Reviews of Sponge Wiper GR-WET

Sponge Wiper GR-WET
Sales Price: 48.99 SGD
Review Rating: 4.57
7 Customer Reviews
5 star 4
4 star 3
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
Cleaning the toilet
5
From Japan
On 2017-11-24 09:52:41
Although I bought it for floor cleaning of the male toilet, it has very strong water absorption capability and it does not have to draw hands, so it is convenient to handle cleanly.
This review is about item#37177987.
Floor cleaning
4
From Japan
On 2016-12-08 14:34:11
I bought it to clean the floor (vinyl plastic? Floor). Although I feel a little heavy, I can use it without problems. If water remains, it becomes slippery and it is dangerous, but here it is good to wipe moisture firmly. Unlike rags etc it is very convenient to drain easily without soiling your hands. Since the diaphragm function is attached to the main body, it is also good that there is no need to purchase separators such as a squeezer like a mop. I used sponge mop for the first time but it was convenient at the moment so I am thinking about additional purchase for cleaning toilet and for use in other places.
Used for floor cleaning
5
From Japan
On 2016-02-10 13:11:19
Although it is used for the floor in general, it is easy to use and easy to manage. Quality is also satisfactory enough.
This review is about item#37177987.
Used for condensation removal and draining of the bath
4
From Japan
On 2015-12-02 16:39:34
It feels a bit heavy but it may be a problem if you get used to it
This review is about item#37177987.
It is Suguremono for wastewater treatment by flooding.
5
From Japan
On 2014-09-13 21:26:54
In the event of a storm, it may flood through an automatic door, it will not make it in time for a mop, so I bought it before trying it here, it is very helpful and it is also very popular from the staff, so I bought additional. Suction of water is also good, and since squeezing can be done quickly, wastewater treatment has become easier. The price is reasonable and easy to purchase.
This review is about item#37177987.
Wiping off water after car wash
4
From Japan
On 2014-01-16 13:40:04
It is heavy. Wipe off the water firmly.
This review is about item#37177987.
Cleaning floor tiles
5
From Japan
On 2012-11-13 20:21:01
I tried using it because I wanted to clean up the washing wastewater when washing the floor tile with acid and suck it well. It's good because the suction performance is good and it can be squeezed quickly.
This review is about item#37177987.
1
Customer Who Viewed This Item Also Viewed
Microfiber Mop
Sponge Mop
Water Absorption Mop, Sponge
Silver wiper wide (W) B ST head only
Mop Head Sponge
Silver wiper wide (W) B head only
Sponge Wiper
Sponge Wiper GR-WET Spage
FF sponge mop
MS Sponge Mop