Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Saddle Cover

Saddle Cover
Sales Price: 18.99 SGD
Review Rating: 3.80
5 Customer Reviews
5 star 1
4 star 3
3 star 0
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
Purchase it as a bruise hidden for the bicycle saddle you are currently using.
From Japan
On 2017-07-05 11:27:58
I was worried about the size because I did not see the actual thing, but I felt relieved because I imagined it was almost same as the image.
This review is about item#37591364.
Used for long-distance running on a road bike.
From Japan
On 2017-05-14 17:16:12
I immediately shifted. I fixed it several times. As a countermeasure, I'm thinking about how to use fixed double-sided tape with anti-slip mat at 100 degrees. I feel that the use feeling is like this. I do not attach it to the saddle from the beginning, I try to use it when the seat surface got sore. For some reason, the saddle cover reduces the mobility. Therefore, I will use it at the limit of patience. It might be less damage if you use it from the beginning. Actually, the reason for purchasing this product was because I thought that I could manage my pain somehow when I ran near 200 kilometers. I hope that you can experience the effect if you use it on road bike more than 100 km. Then, saddle height adjustment becomes necessary. There is gel thickness.
This review is about item#37591373.
For myself
From Japan
On 2016-10-07 11:41:24
The saddle was hard and I felt pain in his buttocks even at commuting time of about 30 minutes, but the appearance was also good, and this item that felt the saddle felt was affordable.
This review is about item#37591364.
Running for a short distance
From Japan
On 2015-10-08 07:36:15
It is equipped with Brooks as a lander Truly it has a realistic feeling that the leather is steady and stable in the use of a long time running but it is useful if there is this cushioning property in the case of a ride other than Choi ride or paved road Speaking of the difficulty It takes a long time to tighten the cord too long Postprocessing is a bit disappointing Also the tip pads bend to the right and left Points to fix after attachment can be solved if you use a velcro tape as a supplement with short straps?
This review is about item#37591373.
From Japan
On 2015-08-14 07:37:02
Increase the amount of GEL,
This review is about item#37591364.
Customer Who Viewed This Item Also Viewed
GEL Saddle Cover
GEL Saddle Cover Sport
Saddle Cover for Sports Bicycle
Shock Absorbing Saddle Cover, Gentle Sheets
Saddle Cover
Special Saddle Cover
Saddle Cover
Saddle cover Standard
Foam saddle cover
Saddle Cover
Shampoo bottle
Gel saddle cover