Buy more than* S$200* and get FREE SHIPPING
Due to the maintenance, we will close our website on June/19 9:00-10:00 and June/23 0:00-0:30 JST. All customers cannot shop on our website during the time. Thank you.

Customer Reviews of Slim Work Light 24+1 Led

Slim Work Light 24+1 Led
Sales Price: -
Review Rating: 2.80
5 Customer Reviews
5 star 1
4 star 1
3 star 0
2 star 2
1 star 1
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
Working light
2
From Japan
On 2015-12-10 17:38:01
Magnetic force is too weak to stick. Brightness is right.
This review is about item#37657785.
Automobile, motorcycle maintenance
1
From Japan
On 2015-09-01 18:41:06
It began to use and it broke down in half a year. One LED at the tip pointed, but the 24 LED side no longer brightens. It is regrettable although it was easy to use in a narrow place.
This review is about item#37657785.
Two wheel maintenance
2
From Japan
On 2013-07-26 00:52:46
Although I was very satisfied with the amount of light and ease of use, as with other posts, the nail of the battery broke quickly, it stopped using the tape and continued to use, it stopped lighting shortly afterwards. Since uneasiness remains in durability, unfortunately I began using another thing.
This review is about item#37657785.
Control panel production etc.
4
From Japan
On 2012-09-05 23:25:45
It was too bright to use in the panel work, but the diffusion of light? Or spreading well, I do not feel uneven so it was easy to work. Unfortunately, there were some problems with the battery lid. · Prevent rattling? , The sponge stuck on the back of the lid presses the battery and gaps are opened in the battery, so there are times when the sponge does not light up. · The slide stop notch of the lid is weak, it has broken in 1 week from the purchase and is stopping the tape now. · Since the strap is attached to the lid, pulling the strap or hooking it will cause the lid to open. (← not occurred) Other than the lid, the magnet is weak and drips off as it sticks to the vertical surface. (Is it NG for board work?) Just as there is brightness as a flashlight and good spread of light, I am expecting UP of completeness. PS: Although it is not waterproof, it is a very easy-to-use flashlight for fishing at night.
This review is about item#37657785.
Vehicle maintenance. Lighting for indoor work etc.
5
From Japan
On 2012-04-19 22:21:51
Size Brightness, easy to hold is good. I wanted magnets at the bottom too, the dash disassembly work is small and the brightness is also satisfied
This review is about item#37657785.
1