Buy more than* S$200* and get FREE SHIPPING
Due to the maintenance, we will close our website on June/19 9:00-10:00 and June/23 0:00-0:30 JST. All customers cannot shop on our website during the time. Thank you.

Customer Reviews of LED Built-in Rearview Mirror

LED Built-in Rearview Mirror
Sales Price: 51.99 SGD
Review Rating: 1.00
1 Customer Reviews
5 star 0
4 star 0
3 star 0
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 1 of 1 Reviews
I wanted to be able to watch it back on the bicycle
1
From Japan
On 2015-02-18 12:34:43
There was something different from the explanation and the picture of the product. Although "It is possible to adjust the optimum angle with two 360 ° rotation ratchets", only one place is rotated (vertical axis can not be rotated). So it can not be oriented like the second picture in the usage example. There is something different from the first picture, and there is nothing like the arm (turned button of ratchet?) At the point where the arm bent 90 degrees. "With one-touch release function, easy to remove mirror & LED part" is a critical point, but it is a crucial part, but it is not useful at all because it is loose and immediately goes off. I will return it.
This review is about item#37721695.
1
Customer Who Viewed This Item Also Viewed
Rearview Mirror
Flexible Mirrors
Bike Mirror
Handle Bar End Mirror
Easy Mirror
Illumination Mirror
Flexible Rearview Mirror
Rearview Mirror
Rearview Mirror
MTB Mirror
Rearview Mirror