Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Pp Graduated Cylinder, Short Size

Pp Graduated Cylinder, Short Size
Sales Price: 4.99 SGD
Review Rating: 5.00
7 Customer Reviews
5 star 7
4 star 0
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
Drug measurement
5
From Japan
On 2017-06-26 17:35:08
It is useful because there are not many measuring cylinders of short size. I would like a glass, if possible.
This review is about item#38450115.
Maintenance of the motorcycle.
5
From Japan
On 2017-04-21 00:45:24
It is convenient to measure a small amount precisely. It is easy to use because it can withstand gasoline.
This review is about item#38450081.
Weighing compressor oil
5
From Japan
On 2016-03-26 13:39:37
Currently, there is a work to add 25 ml of compressor oil in the recall operation of the car, since we had just 25 ml measuring cylinder we bought it. Since I did not have such a small graduated cylinder, I got work done after purchasing this cylinder. I understand that it is better to use the proper size even though the large is doubly small.
This review is about item#38450072.
Candle mold
5
From Japan
On 2013-07-30 08:57:14
The application is totally different, but I use it for the candle type. Exclusive ready-made goods are expensive so they are cheap, durable and very helpful. Also, the sense of stability is very good as the hem is quite wide.
This review is about item#38450115.
It is used for weighing mixed oil and front fork oil.
5
From Japan
On 2013-06-19 18:27:08
It is a short length, so it is a barrel, it is natural, but ^ ^;
This review is about item#38450115.
Used when exchanging fork oil of a single vehicle
5
From Japan
On 2013-05-20 22:34:57
Since it is not made of glass, we do not have to worry about falling. The mouth is easy to pour large.
This review is about item#38450115.
Identify the weight of fertilizer
5
From Japan
On 2013-05-09 22:48:47
I am using it without problems.
This review is about item#38450124.
1
Customer Who Viewed This Item Also Viewed
TPX GRADUATED CYLINDER
Fine Graduated Cylinder
Poly Measuring Cylinder
Polycylinder
Fine Chemical Cylinders
Polycylinder
Liquid Meter Cylinder Type
TPX graduated cylinder
Chemical graduated cylinder
PP graduated cylinder
PP graduated cylinder
Liquid meter cylindrical type
Measuring Cylinder
Measuring Cylinder