Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Basic Switch D2RV

Basic Switch D2RV
Sales Price: 5.99 SGD
Review Rating: 2.50
2 Customer Reviews
5 star 0
4 star 0
3 star 1
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 2 of 2 Reviews
For lighting control at door opening / closing
2
From Japan
On 2018-01-26 09:11:53
Sorry, I did not check the item well, but there was a fault but the contact composition was different. Even if you look at the picture, the terminal part can not be seen clearly. I wanted 1b contacts, but this is lit once I close the door to open the door when I close it, and I am a relaxing one. Even if I looked at the product page many times, the contact composition was not described and confirmed by the manufacturer HP. The item itself is a good one and there is nothing wrong, but since it was not listed on Mr. Monotarau's HP, I made it to 2 ★. I'd like you to describe the contact composition as well.
This review is about item#46525114.
Extended switch to pointing device.
3
From Japan
On 2014-12-01 12:44:39
Although it is not mounted (I used the same D2VW sealed type), I think that it is optimal without problems. If the lever is longer than this (lever ratio large), I think that the load is too low. Conversely, in the case of game machines and the like, would it be better to have a load? .
This review is about item#46525087.
1