Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Entrant Raincoat

Entrant Raincoat
Sales Price: 85.99 SGD
Review Rating: 4.00
5 Customer Reviews
5 star 3
4 star 1
3 star 0
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
Raincoat for bike
5
From Japan
On 2017-01-19 05:22:46
Very good as a raincoat for bike. Compared to the separable type, you can easily wear even in the rain. Since the triangular part of the foot is independent with zipper, it is easy to handle, and feet are protected from rain. There will not be any more.
This review is about item#38584402.
Used for motorcycle commuting
5
From Japan
On 2016-01-27 20:00:14
I have not used it once but it is light and easy to wear. Although I feel a little expensive, I am satisfied because both water repellency and breathability are good.
This review is about item#38584515.
School work
5
From Japan
On 2015-09-18 21:58:14
I bought myself and was very good so I purchase 2 for my son. I think that the size is somewhat big, but I think that you can wear comfortably. It flips the rain water flawlessly. I think that it is very good. It is recommended for those riding bicycles and motorbikes.
This review is about item#38584341.
Used with two mopeds at 20 km / one average speed of 50 km / hour
1
From Japan
On 2012-12-29 02:15:19
It does not function as a raincoat with the above use. It's normal rain. I will inevitably flood from my chest zipper part. Although it seems that there is "return" in front, it seems to be small and not functioning. A straight spot can be made in the middle of the shirt. It is a defective item that can not bear the usual rain, although it costs a reasonable price? I am worried whether it is a defective item just because the review of the other person was good. It is not likely to endure at least scooters and bicycles. It is very disappointing because there are no other parts including materials. It may be able to go with drizzle or light rain, but it seems to be difficult on a scooter. I would like to return if it is not possible to return goods. It is impossible to make it at this price.
This review is about item#38584524.
For cold weather at commuting time
4
From Japan
On 2011-12-25 20:36:14
I was attracted by the length of the length and the leg part conscious of riding the scooter and purchasing it. In cold weather, pants and front wear may be higher, but one piece type is the best, considering the convenience and appearance of detachment. Although the product name was a raincoat, I was worried about cold weather a little, but I did not feel it bitternely, even if I was traveling at about 50 km / h speed in the morning of 5 degrees Celsius. When folding, it is also nice to enter the helmet storage part cleaner.
This review is about item#38584357.
1
Customer Who Viewed This Item Also Viewed
PVC Colorful Rain Coat
Rain Alpha
Long Rain Coat
Safety Rain Suit
Rainware,
With 2WAY cycle coat leg cover
Entrant Rain Suit
Motorcycle raincoat
salsa
  • salsa
  • Tohkemi
  • 57.99 SGD
Rainbow
Waterproof long coat
EVA Poncho
Rain Poncho