Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Easy Mirror

Easy Mirror
Sales Price: 21.99 SGD
Review Rating: 4.00
9 Customer Reviews
5 star 4
4 star 3
3 star 1
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 9 of 9 Reviews
On a bicycle
4
From Japan
On 2017-04-16 01:21:45
Because it can be folded and stored, it is appreciated when parking. It is easy to see with a wider view of the back. Because it is chrome treatment to plastic, it comes bald for about 2 years. Black was better! Is it?
This review is about item#38626016.
Bicycle mirror
3
From Japan
On 2016-06-26 09:21:53
I bought it because the bicycle purchased did not have a mirror. Although it was smaller than I thought, it seems that it is not narrow enough that the viewing range becomes problematic. The installation is wrapped around the handle bar, but it is hard to do because it is very tight when adjusting the mirror. It would be nice if you feel a little more clicking.
This review is about item#38626025.
When driving a bicycle
1
From Japan
On 2016-04-17 21:47:59
The metal that I put in the first place (trumpet shape) was only slightly (about 1 mm) big and I could not enter the handle end of the bicycle. Because it was lead, I bought a metal file and cut it a bit. It was a part whose inspection of products was not done.
This review is about item#38626034.
Worn on a bicycle
4
From Japan
On 2015-09-18 17:58:55
It was okay if it was a catalog that could confirm the status of wearing
This review is about item#38626025.
Attach to the tip of the drop handle
5
From Japan
On 2015-05-19 09:19:45
A moderate field of vision and good shooting without blurring are good. Mounting on the bar end is securely done, and there is no problem fixing the position. I felt the degree of freedom of the angle less first, but if you tighten it moderately, you can easily fix the position when hitting something, no problem. As a whole impression very well, I will repurchase it even if I break it by something.
This review is about item#38626025.
For my car
5
From Japan
On 2014-05-08 12:38:14
Since the curved surface ratio of the mirror surface is small, it is easy to grasp the distance feeling. I made the color chrome, so the light of the oncoming car reflected, maybe it is safe? I bought without measuring the inner diameter of the handle, so it was processed somewhat, but it was installed fairly. However, the moving part is too clown. Just a bit of touch makes the angle slip. I wish I had become a little more jealousy.
This review is about item#38626016.
Bicycle rear view mirror
4
From Japan
On 2014-04-02 15:01:48
The convexity of the mirror looks good just fine. The mirror fixing screws are ineffective, and it is a bit of a difficulty to tighten them quite strongly.
This review is about item#38626025.
Commuting bicycle
5
From Japan
On 2014-01-19 13:57:36
Mirror surface has good curvature, easy to grasp in the back. Also, since it is easy to install and remove, it is very convenient for us who are using MTB and road bike together for commuting.
This review is about item#38626025.
Used for MTB
5
From Japan
On 2013-07-15 21:53:25
It is attached to the MTB bar end and it is used. I am also very satisfied with the reflection on the back. Since it is attached to the bar end, it is compact and it does not block visibility. I am planning to install it on a road bike this time.
This review is about item#38626025.
1
Customer Who Viewed This Item Also Viewed
Rearview Mirror
Flexible Mirrors
Bike Mirror
Handle Bar End Mirror
Illumination Mirror
Sport Pedals
Color Rearview Mirror
Rearview Mirror
Flexible Rearview Mirror
Rearview Mirror
Rearview Mirror
MTB Mirror
Rearview Mirror
Bar End Mirror
Rearview Mirror