Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Solenoid Valve, Momotaro II) Piston System

Solenoid Valve, Momotaro II) Piston System
Sales Price: 329.99 SGD
Review Rating: 4.90
10 Customer Reviews
5 star 9
4 star 1
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 10 of 10 Reviews
Use water for control valve of equipment to raise up to 160 ℃
5
From Japan
On 2018-05-01 09:20:18
For the time being, it works without problems, but how long you can withstand long-term use is an issue.
This review is about item#35026573.
Piping work
5
From Japan
On 2016-08-24 14:21:01
Especially it can be used without problems. I think that I will work smoothly.
This review is about item#35026591.
Used when steaming the washing machine
5
From Japan
On 2016-06-07 17:08:58
It is good that it can be used even at 100 V or 200 V
This review is about item#35026607.
Opening and shutting of steam piping
4
From Japan
On 2016-04-06 11:00:29
It was still better if there was only the electric part at the top of the solenoid valve.
This review is about item#35026616.
To maintain set temperature
5
From Japan
On 2015-10-17 00:36:17
I was using Momotaro and I was looking for the same thing but I was Momotaro 2 so I bought it Because I have not changed it yet I do not know the details but since there is considerable strength in replacement, stainless steel I wish I had a product made
This review is about item#35026582.
Piping of fuel tank filling section.
5
From Japan
On 2015-03-24 19:16:25
It was a very satisfactory product.
This review is about item#35026625.
As a stop valve for steam from a boiler
5
From Japan
On 2013-11-25 14:54:06
Compact and where coils are common.
This review is about item#35026607.
Used for sprinkling at plant
5
From Japan
On 2013-10-30 18:19:22
It was the same as having used things before
This review is about item#35026582.
Steam line
5
From Japan
On 2013-05-31 08:23:01
Easy to use because the voltage is shared between 100 and 200 V. Delivery times are useful quickly.
This review is about item#35026591.
Temperature control
5
From Japan
On 2013-04-01 09:41:40
The product operated without problems, it was safe to use.
This review is about item#35026591.
1