Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Ball Valve Made of Brass, Butterfly Handle, Reduced Bore

Ball Valve Made of Brass, Butterfly Handle, Reduced Bore
Sales Price: 10.99 SGD
Review Rating: 4.40
5 Customer Reviews
5 star 3
4 star 1
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
As a valve for drain piping
3
From Japan
On 2016-11-11 21:42:43
The surface finish of the hexagonal part of the main body is a bit miscellaneous, it does not go far to Bali, but it catches on your fingers when you have it. It was lightly sanded and used.
This review is about item#38657823.
To self-made Air Blow gun valve
5
From Japan
On 2016-08-05 20:13:35
Open, closed position is clear, compact and usability is very good product. I will also purchase it.
This review is about item#38657814.
For air piping
5
From Japan
On 2016-02-04 09:02:15
It is compact and easy to use.
This review is about item#38657814.
Old car's heater valve
5
From Japan
On 2013-07-03 20:48:36
I use it as a very inexpensive alternative part. Product is also sufficient thing.
This review is about item#38657832.
Compressor air line
4
From Japan
On 2013-04-09 06:50:14
It is used as a drain valve of a compressor (0.75 kw) for DIY. It is informed that it is not an ideal way to use a ball valve, because it is set to a slightly opened position when discharging drain. The handle of the valve seems to be made of plastic and it is not possible to deny the possibility of turning to force hands and breaking it when the valve body is deteriorated and hard. However, it was small, so it could be installed in a narrow (under the tank).
This review is about item#38657823.
1