Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Centerless Ground Rod

Centerless Ground Rod
Sales Price: 1.99 SGD
Review Rating: 4.33
6 Customer Reviews
5 star 5
4 star 0
3 star 0
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
I use it for the work.
5
From Japan
On 2018-02-09 14:42:18
I bought it because I wanted a shaft thing that would fit exactly in a 17 mm hole. It is correct answer by purchasing skillfully.
This review is about item#38806354.
Pillar connection for agricultural work
5
From Japan
On 2017-05-18 18:32:42
Packaging was solid, so we could use it with confidence. It took a little time for the delivery date, but ,,,
This review is about item#38806397.
Inspection jig at product inspection
5
From Japan
On 2017-05-18 10:52:05
Material: I am satisfied with both dimensions. Because it takes time to cut, I would like you to increase the size (L size).
This review is about item#38806171.
Substitution of damaged bicycle brake parts
5
From Japan
On 2016-01-14 15:10:36
I purchased plastic parts of about 4 mm * 9 mm which was used for the spring bearing of the caliper brake to substitute it. The accuracy is good and the strength seems to be enough. However, although it was necessary only 9 mm in length, there was something to think though there was no choice but to distribute it separately in a box of 130 cm in 1 m unit.
This review is about item#38806074.
To create parts for electric / model work parts · · ·
1
From Japan
On 2015-12-06 22:00:05
Although Φ 17 mm also has a thickness, it is bent by 1 to 2 mm at 1000 mm. It seems that there is considerable problem in storage / storage method. (If it is leaned up and stored and stored, it will bend with gravity.) If you do not store and preserve such products without fail, it will bend all regardless of thickness.) If you are bent right after manufacturing, minus tolerance It is better to have no items. If there is no bend in the lathe, if you scrape tolerance - 0.1 mm or less, it becomes thinner 2 ~ 5 mm than purchase size. Even though it is an outer diameter product that can be used without precision cutting, there is no point in being bent.
This review is about item#38806354.
At the do-it-yourself carpentry manufacturing stand holder of 3/8 socket tool
5
From Japan
On 2015-05-08 04:49:25
I bought it because I was looking for an affordable plaque to add to an existing plastic holder.
This review is about item#38806171.
1
Customer Who Viewed This Item Also Viewed
PTFE Round Rod
White Round Pipe
White ABS Round Bar
POM-NH, Homopolymer, Round Bar
POM round bar
MC801 (weather-sliding grade) round bar
MC801 (weather-sliding grade) pipe
MC501CD R2 (conductive grade) round bar
POM-NC Nylon Pipe
POM-NCHY (hyper) round bar
PET100 (natural grade) round bar
U-PE100 (Natural grade) round bar
MC703HL (slide grade) round bar
Resin Round Bar
Resin Round Bar