Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of POM-NH, Homopolymer, Round Bar

POM-NH, Homopolymer, Round Bar
Sales Price: 4.99 SGD
Review Rating: 3.33
6 Customer Reviews
5 star 3
4 star 0
3 star 0
2 star 2
1 star 1
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
For work
5
From Japan
On 2016-08-25 22:51:23
It is user-friendly and satisfying with price.
This review is about item#38807632.
Hobby · Crafts
2
From Japan
On 2016-03-24 17:24:09
Although it seems to be translucent in the image, the real thing is white, and coloring is difficult to say semi-transparent. I would like to ask the image faithfully to the real thing.
This review is about item#38807632.
Maintenance parts for food processing equipment · To create parts ...
2
From Japan
On 2015-12-06 22:19:41
The surface is dirty. I wiped it with something's chemicals and it seemed like I was not wiping it dry, there was a trail of drooling in the whole. As after shaping, the surface gloss is dirty. Although it says "parts requiring sanitary properties such as food processing machines and medical equipment parts" for use, there is considerable hygiene problem in the extent that it is wiped off with detergent or alcohol unless surface treatment is done. It was a product that was not bent by POM round bar.
This review is about item#38807754.
Jig Production Material
1
From Japan
On 2015-11-26 11:59:16
Although it was an opinion that I watched the review and said that it did not need worry such as bending, I bought it because I was concerned that buying one was okay. Then it was 1000 mm of 30 mm this time but the bending was so bad that I could not use it. It was that it was within the permissible range where you sent photos of bending and listened. I bought three books, I felt it was okay for two, I feel that one is clearly different, I think whether it is too complicated if this is acceptable. Because we can not accept returns or refunds, we have only got to throw it away. I think that the quality of the product is good, but it does not become usable with such a complicated processing. I'm sorry.
This review is about item#38807781.
Material of prototype
5
From Japan
On 2015-04-28 15:25:40
Accuracy comes out, so it's easy to use.
This review is about item#38807623.
I used it as a stocking material for push buttons
5
From Japan
On 2014-03-14 15:39:08
I was curious about bending etc because it was a resin long, but I was worried about it. I was also concerned about what kind of packaging it would deliver, but I was in dedicated packaging and there were no scratches. I bought φ 10 mm, but I think that the real thing is slightly larger than 11 mm in thickness, and it can be used for applications that can not be used under 10 mm. If possible, I think whether there is a cutout from about 50 cm instead of 1 m.
This review is about item#38807702.
1
Customer Who Viewed This Item Also Viewed
Teflon Round Bar
MC Nylon MC901 Round Stock
PTFE Round Rod
White Round Pipe
White ABS Round Bar
Urethane Round Bar
MC901 Nylon Pipe
POM round bar
Centerless Ground Rod
POM-NC Nylon Pipe
POM-NCHY (hyper) round bar
PET100 (natural grade) round bar
Resin Round Bar
Resin round bar