Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Lightweight Clutch

Lightweight Clutch
Sales Price: -
Review Rating: 3.83
6 Customer Reviews
5 star 2
4 star 1
3 star 3
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
Repair exchange
4
From Japan
On 2015-09-03 00:02:24
It purchased for repair of Taiwan made KYMKO 50 cc suna-Z. Since Kimco was tied up with Honda, I bought a thing for Live DIO. Since it is a lightweight clutch, it will be connected at high speed range, so Weightroller also bought 9g items at the same time (Puriri replaced with High Speed), but I installed it better than I thought Although it was replaced with 8 g, it was improved. Before exchanging the clutch, I only got 65 km (meter reading), but after replacing it was in parallel with the car and it was up to 77 km. (It is a violation!) I think that it is excellent for cost performance. It is an improvement point, but it was better if we could exchange the spring without removing the clip.
This review is about item#39188852.
On clutch wear
3
From Japan
On 2015-01-21 16:06:02
I used it for repairing Dio AF 28 ZX It is slightly lighter than the normal clutch but worn as it would be okay From the nature of the lightweight clutch the timing to connect became late and the sky rash at the time of transmission increased
balance
5
From Japan
On 2014-05-01 20:10:27
He writes that he was disappointed with another review. It seems that the performance balance has gone wrongly by making it a light speed clutch with a high speed pulley. WR became very satisfied with 8.5 × 3, 8.0 × 3. It was good to purchase.
Performance of AF 27 UP
3
From Japan
On 2014-04-06 07:18:23
I exchanged the old AF 27 pulley with a high speed pulley, so I bought it expecting this item, but in conclusion, there was no difference that I could experience with a normal clutch before replacement. Satisfaction with expectation ☆ Price satisfaction ☆ 1 piece.
This review is about item#39188852.
Weight reduction of genuine clutch
5
From Japan
On 2013-09-04 12:55:20
It was diverted to 5FA6. Thickness is a little thin, but the area of ​​the shoe is the same, the rotation speed of the clutch meat has increased. It can be used without any problem.
This review is about item#39188861.
Used for bike remodeling
3
From Japan
On 2012-05-30 20:16:22
Weight is 640 g, but when we measured it it was 605 g. Actually I wanted something of 640 g, so it was a bit disappointing. People who purchase this hand think that they are looking for severe things, so I think that it would be better to fix it. I think that it is good that the price is cheap!
This review is about item#39188861.
1
Customer Who Viewed This Item Also Viewed
Pulley
Weight Roller
Slide Piece
Lock Nut Wrench
Pulley Kit
Clutch Weight ASSY
Normal Clutch Spring
Clutch Center Spring
Clutch Center Spring
Clutch Assembly
Clutch Assembly
Clutch Shoe Kit
Clutch Shoes