Buy more than* S$200* and get FREE SHIPPING
Due to the maintenance, we will close our website on June/19 9:00-10:00 and June/23 0:00-0:30 JST. All customers cannot shop on our website during the time. Thank you.

Customer Reviews of Arbor

Arbor
Sales Price: 12.99 SGD
Review Rating: 2.93
15 Customer Reviews
5 star 5
4 star 1
3 star 2
2 star 2
1 star 5
The reviews are automatic translation.
Showing 1 - 15 of 15 Reviews
Drilling work of woodworking
5
From Japan
On 2018-05-30 10:30:54
This product is used with the set of Baico's bimetallic horso. In addition, there are many items of bimetallic holster. Although the hole saw is generally expensive, I think that it is convenient to be able to match various bore diameters at relatively inexpensive by replacing the bimetallic horso.
This review is about item#39386146.
Drilling of metal siding
2
From Japan
On 2018-05-08 20:32:49
As the others are written, the center drill will loose and fall during drilling. I wonder if it is better to attach with an adhesive? Especially it will come off as soon as clutch and vibration come out.
This review is about item#39386173.
Drilling walls part 2
1
From Japan
On 2018-04-24 11:47:23
I wrote important things so I will add it. Since 65 mm Holsoau's teeth and the tip of the center drill are Tsuraichi, the hole drilling position will be displaced completely. At least the tip of the center drill needs to be 5 mm or more. I do not even know that the center drill was a short defective item only for individuals I bought ...
This review is about item#39386155.
Drilling on the wall
1
From Japan
On 2018-04-24 11:30:52
Used when drilling air conditioning piping on gypsum board. Within three minutes, the center drill passed, in addition, quick fixation of the immobilizer screw was released and the arbor and the Holso were attached firmly. Since there is no Japanese in the instruction manual, I do not know what I should pay attention to at the beginning of use, I think that it is the obligation of the distributor to attach Japanese instruction manual. Since Holso is a waste, I am planning to purchase Arbor which is not quick again, but since the sharpness of Holso is not a good one, I personally recommend a different item. To be honest, I had better not buy it ...
This review is about item#39386155.
When drilling work
5
From Japan
On 2018-04-23 23:09:30
Cost performance is very good. Usability is also good.
This review is about item#39386173.
Drilling in an iron box such as a switchboard
1
From Japan
On 2018-03-25 16:19:46
After penetration of the center drill, the core broke from the moment the hole saw stuck and can not be cut well. After checking, the center drill was bent. I can tell if it will break, but is it a material that is a bending drill? this. It was disappointing with this for a first drilling operation.
This review is about item#39386137.
Iron: Drilling of about 1.6 mm
4
From Japan
On 2017-02-27 10:19:40
There is a problem with not being able to order only drill parts of expendable parts.
This review is about item#39386146.
Air conditioning construction
5
From Japan
On 2016-08-16 11:31:05
I purchased this type of shank for the first time. I think that it seems easy to do just by sliding exchange of Holso. Although it is also in the review of others, it may be necessary to pay attention so that the embedded hexagonal screws do not come off by vibration ...
This review is about item#39386173.
Docomo antenna construction
3
From Japan
On 2016-07-27 16:32:48
I would like you to sell the center drill and other parts separately. Because the blade of the center drill fell into the wall and it lost when using this product the first time, I want a spare blade replacement
This review is about item#39386182.
Plumbing wall opening
3
From Japan
On 2016-05-28 07:10:55
The immo Screw stopping the moving part got off by the vibration during work and the spring and the ball flew away. I am repairing with vinyl tape and using it. Without this part it will be hard to remove the core. It is a place I want to devise that I can not remove the screw.
This review is about item#39386173.
Drilling of woodworking work
5
From Japan
On 2015-11-08 18:11:14
It is slightly different in structure from the one we already have in USA, but versatility is satisfactory enough. In item description, please describe the size in detail such as distance between lock holes. It duplicated what I already have.
This review is about item#39386146.
Drilling into steel pipe and SUS pipe
2
From Japan
On 2015-01-13 00:07:44
Because the screw to stop the center drill is a minus screw, it takes a lot of hardship in case it becomes necessary to replace it due to breakage of the drill etc. Since the screws themselves are M8, I decided to use them for Hex's things, but at other companies, including domestic manufacturers, this part was first a hex, so I felt the difference in the way of thinking (culture) with Europe. The sharpness of cutlery is not bad, and because it is inexpensive, our company has increased the size of the blade little by little and the usage rate is expanding.
This review is about item#39386155.
Hold Holsau and open 68 holes
1
From Japan
On 2014-09-16 21:16:55
I tried to loosen the screw with a flat head screwdriver to replace the dust of the center, but there was no loose appearance, even if I loosened with the impact driver I thought that the minus breaks and does not loose, I thought about the exchange, but the thing unpacked I bought a variety of products so far, but from now on I thought that I should think about buying tools. Goods that do not loosen the screw are bad. (Kiri of the center can not be replaced)
This review is about item#39386155.
Installation of hole drilling board etc.
1
From Japan
On 2014-02-02 19:10:30
Although it is a matter of Baccoa, although there is a spring between the points where it is hexagonal, I think that it is better to close all with a hexagon Holster is displaced
This review is about item#39386155.
External wall drilling
5
From Japan
On 2013-01-08 12:12:42
It could be used for both structural plywood and galvanized steel sheet.
This review is about item#39386146.
1
Customer Who Viewed This Item Also Viewed
Bimetal hole saw
Bimetal Hole Saw Set
HSS Hole Saw
FCL Hole Cutter
Bimetal Hole Saw J Shaped
Bi-Metal Hole Saws
Magnetic card case
Adapter