Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Pig Leather Gloves, Piggy PLUS, Athlete F-505

Pig Leather Gloves, Piggy PLUS, Athlete F-505
Sales Price: 10.99 SGD
Review Rating: 4.60
5 Customer Reviews
5 star 3
4 star 2
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
During metal processing
4
From Japan
On 2016-12-06 17:55:28
Especially the fingers of the thumb and index finger tend to be torn as it is used during metal processing.
This review is about item#39576196.
Electrical construction
4
From Japan
On 2016-10-31 19:26:44
It is a repeater. Since it will not become hard even when washed, it can be used for a long time. In addition, the price is relatively low-priced sewing firmly, there is almost no solving from the sewn part. I am using LL because my fingers are long, but since the surroundings become fluffy, I am glad that there is a type of slim LL length.
This review is about item#39576205.
Grass cutting work etc.
5
From Japan
On 2015-10-06 20:53:32
I used a pig leather magic glove, leather was just fine with good hardness I think that I would like to buy from now on.
This review is about item#39576266.
Logistics light work
5
From Japan
On 2015-03-10 21:50:21
It is a soft leather and glove including fingers as a whole, there is no hit due to sewing etc and the feeling of fit is very good. Because the thickness of leather is slightly thin, it is unsuitable for hard work but handling such as fork operation and handwriting with wearing gloves can be done smoothly.
This review is about item#39576205.
For automobile / motorcycle maintenance and for motorcycle gloves
5
From Japan
On 2014-10-04 19:24:06
I purchased and used various pig leather gloves as working gloves, but I felt that this product was the best fit and easy to use. Moreover, it is cheap. Because the leather is soft and the part of the instep has become a stretchy mesh, there is nothing like stretching even if you bend your fingers and sewing is exquisite without steaming so that the seam at the tip of the finger may be scratched There is none. Small screws are also very easy to grasp. It is a very good product, so I would like to use it when riding a motorcycle. Although it is cheap, it is real leather, so I think that the safety when rubbing is more than cheap bike gloves made of synthetic leather is much higher.
This review is about item#39576214.
1
Customer Who Viewed This Item Also Viewed
Swine Leather Gloves
Pig Leather Work Gloves, Knitted
PU Globe
Swine Leather Gloves
New cell Let aluminum kettle
PH-301 Blue
Pig Leather Gloves
Cow Leather Gloves No.12A
BF-102 break fit
F-505 Green S
F-505 Gray L
Razorsaw Fold Universal Replacement Blade
Fitton PRO