Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of D-type rubber

D-type rubber
Sales Price: 3.50 SGD
Review Rating: 4.40
5 Customer Reviews
5 star 2
4 star 3
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
To the parking lot cushion
4
From Japan
On 2017-06-29 11:31:22
It seems to be outdoor durable material. I felt that the double-sided tape seemed to come off, so I used an adhesive together.
This review is about item#39583074.
As a damper for free access floor tiles
4
From Japan
On 2017-06-14 15:53:52
It was able to be used without problems. However, it is saved if there are variations in length.
This review is about item#39583083.
Prevent wires from collapsing
5
From Japan
On 2015-12-14 00:32:40
It is cheap and good.
This review is about item#39583083.
Used cusually as a light truck carrier
4
From Japan
On 2014-09-17 15:30:44
The light tiger's deck is painted, but it is a steel plate, there is no cushion, so it gets scratched, the loading table is full of scratches. "Worrying matter" D Although rubber has an adhesive material, I am worried how long it will have durable adhesion. Currently in use while worrying about durability. that's all
This review is about item#39583074.
Roof carrier
5
From Japan
On 2013-12-03 13:06:49
I used it as a cushioning material for the roof carrier of the car. It is a snug fit because the width is 30 mm wide. I drilled a hole and it was stopped with a tie wrap. I also put a surfboard just as hard.
This review is about item#39583083.
1
Customer Who Viewed This Item Also Viewed
Cord Cover
Easy Grip
Cushions Semicircular
Cushion Half-Moon-Shaped
Car Stop
NEO Stopper
Bumper professional
Safety Corner Cushion
Safety Corner Cushion
D-type rubber
Car Stop With Hole
Safety Corner Cushion