Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Double Ring Ratchet Combination Wrench

Double Ring Ratchet Combination Wrench
Sales Price: -
Review Rating: 4.11
9 Customer Reviews
5 star 4
4 star 3
3 star 1
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 9 of 9 Reviews
Bicycle assembly
4
From Japan
On 2015-04-20 10:27:26
The ordered item is slightly bigger than the one we used before, but the head of the ratchet is bigger and durable feeling, but usability at the narrow place is a bit less usable, because the head portion of Latchet is big. In the case of tightening about 8 mm / 10 mm, the torque is low, so it is best if the ratcheting part becomes smart a little more.
This review is about item#40130011.
Maintaining a hobby's racing cart
5
From Japan
On 2015-01-19 21:26:46
Made in Italy most racing carts are special in screw size, not M12 and M10 is M13. On the other hand, ordinary combinations are M10 × M12 and M11 × M13. Even if I looked for anywhere, there was no ratchet M10 × M13 combination, but Monotaro had it! I'm happy to buy it immediately and it is useful. If it is greedy, it is the highest without complaints if it is a head swing ratchet, can not you be commercialized?
This review is about item#40130027.
Tightening work of steel etc.
5
From Japan
On 2014-10-17 19:57:43
I use it pretty, but it has not been crushed yet. I would like to buy it as soon as I use it and continue to use it.
This review is about item#40130036.
Bolt tightening
4
From Japan
On 2013-05-12 16:01:37
The price was higher than when I last bought it. Somewhat, the bearing feels firm. Last time was better. However, since it is easy to use, please do not discontinue it.
This review is about item#40130036.
Vehicle maintenance
3
From Japan
On 2013-03-22 19:25:43
I think that I am comparable with other manufacturer products especially when using it to the present.
This review is about item#40130036.
Auto Repair
2
From Japan
On 2013-03-22 17:52:43
Since the ratchet is stiff, it comes with a nut when returning. There was no problem at the time of tightening.
This review is about item#40130027.
Vehicle maintenance
5
From Japan
On 2013-03-09 09:52:33
The feeling of use is very satisfying for now. The weight is also quite good.
This review is about item#40130011.
Installation of sanitary ware etc.
5
From Japan
On 2013-01-24 17:14:10
I think that I am comparable with other manufacturer products especially when using it to the present. Because there is a reasonable wall thickness, it feels a bit heavy, so if the size (length) is a bit smaller then it is convenient to use
This review is about item#40130027.
Sliding door mounting screw (narrow area) and pulley mounting screw section
4
From Japan
On 2012-12-25 10:05:10
It is cheap and structurally cheap because you can choose left and right rotation on the front and back.
This review is about item#40130027.
1
Customer Who Viewed This Item Also Viewed
Ratchet Face Ring Spanner
Flex Head Gear Wrench
Ratchet Box End Wrench
Ratchet Offset Wrench
A Ratchet Wrench With An Angle
Super Gear Wrench, Straight
Short Gear Wrench
Double Flex Gear Wrench
Glasses Giarenchi
Gear Wrench
Ratchet Offset Wrench
4 Size Ratchet Wrench
Combination Wrench
Gear Wrench