Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Transparent ABS Round Pipe

Transparent ABS Round Pipe
Sales Price: 1.54 SGD
Review Rating: 4.20
15 Customer Reviews
5 star 9
4 star 2
3 star 3
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 15 of 15 Reviews
Material of work
5
From Japan
On 2017-12-08 15:29:24
It was convenient to use conveniently. It is cheap and is the best.
This review is about item#40357387.
I wanted a transparent plastic pipe and it was able to be applied.
5
From Japan
On 2017-05-29 15:13:44
The price was cheap, and we were able to do work as expected.
This review is about item#40357362.
Work making
3
From Japan
On 2016-09-30 19:33:15
Thank you for your prompt response. It was affordable as well.
This review is about item#40357387.
Used for underwater robots
5
From Japan
On 2016-09-30 08:20:56
When passing the cable through the cable gland, in order to secure the strength when tightened up, once the cable is passed through the ABS pipe and hardened with epoxy bond, tightening this ABS pipe with the ground will not cause water leakage.
This review is about item#40357371.
Fishing rod parts
5
From Japan
On 2016-09-19 17:07:24
Since a pipe case is not attached unlike Ayu Rod, # 1 / # 2 parts of the mountain stream mainstream pole is thin, long and easy to break, so purchase. I am glad that this length is incomplete.
This review is about item#40357362.
Golf 2
4
From Japan
On 2016-09-12 12:57:40
Inner diameter 8 Outside diameter 10 Can be used for repairing door locker pins such as golf 2
This review is about item#40357371.
Mechanical auxiliary equipment
1
From Japan
On 2016-08-05 04:01:06
I purchased a product with an outer diameter of φ8. If I tried to insert it in a hole-drilled place with 8 mm bit size did not match at all ... I thought it was strange and I measured the size and it was 8.2 mm. There is no reason for drill bits of 8.2 mm, so you have to throw them away. I think that it is not an acceptable tolerance at all.
This review is about item#40357362.
distillation
5
From Japan
On 2016-08-02 23:36:07
I use it with a perforated rubber stopper.
This review is about item#40357396.
Used for piping of air and CO 2 in the aquarium at home
3
From Japan
On 2016-04-13 17:49:29
Up to now, two air piping and one CO 2 piping in the 90 cm water tank at home were piped with a hard vinyl tube, but after all the vinyl tubes could not be piped straight in the tank due to bending streaks I was inevitably looking because I was fixing with many kiss rubbers. I bought this product according to the tank reset, bent it by a dryer according to the shape of the aquarium, and used it for the substitution of a vinyl tube. Since there is no difference between vinyl tubes, it is possible to drastically reduce the number of fixing kiss rubbers and it was only pleasant that the appearance changed and it was only for 2 months. I need to regularly exchange AirStorne and CO2 stone, but when trying to remove the stone connected by a silicon tube at the time of the first stone change, it was easily broken as "Pokit." It seems that the water temperature in the aquarium is always 26 ° C, but it seems that the ABS resin became brittle under low temperature water only for only two months. Although it was not originally made with such assumption in the first place, despite choosing an ABS resin pipe which should be strong against ultraviolet rays and heat, it is very disappointing that it has become the result as a result.
This review is about item#40357396.
Machine auxiliary parts
5
From Japan
On 2015-12-18 14:51:28
Anyway, the size is plentiful, because it is made of resin, it is easy to do a little processing
This review is about item#40357353.
Alignment for pop pasting
4
From Japan
On 2015-11-20 15:00:46
It was translucent than I expected. The material was soft and comparable, it was easy to process. The price is also cheap, I think that it is good for a lot of people using it.
This review is about item#40357353.
It is used for self-made of an insect tube.
5
From Japan
On 2015-05-17 19:37:25
It is good to use for a pipe which sucks small insects. I used a pipe with an outer diameter of 6 mm. The pipe of 5 mm was good to use for connecting people who breath. I wanted one more pipe too.
This review is about item#40357353.
Carbon dioxide piping in aquarium
3
From Japan
On 2015-03-16 22:59:42
The piping of carbon dioxide which had been handling with the silicon tube was replaced by a round pipe. It is good to look shabby. It was hard and tough to cut with a pipe cutter for silicone tubing. Although it is natural, recommended cutting tool special tool.
This review is about item#40357353.
Model aquarium
5
From Japan
On 2015-03-16 17:38:42
I am saved because 5mm handles few places.
This review is about item#40357396.
Piping relationship
5
From Japan
On 2014-10-08 22:14:26
It is a dish that is easy to process and attractive in terms of price.
This review is about item#40357353.
1
Customer Who Viewed This Item Also Viewed
Acrylic Pipe
Urethane Pipe
FEP Tube TF145
Black Round Pipe
White Round Pipe
White ABS Round Bar
POM-NH, Homopolymer, Round Bar
FEP Tube TF225
Aluminum Round Pipe
Pipe, Semi-Slit
Pipe binder
POM-NC Nylon Pipe
Jun Freon FEP Tube (TF 085)
Transparent TS joint socket
Micro Scissors