Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Active Conditioning Filter

Active Conditioning Filter
Sales Price: 42.99 SGD
Review Rating: 4.43
7 Customer Reviews
5 star 3
4 star 4
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
Car oil filter change
5
From Japan
On 2017-11-12 22:51:11
It is unknown what exactly how it works, but it seems that washing inside the engine and fluid resistance decrease occur as described in the product, engine which has already traveled 190,000 km is quiet like the new car It began to turn smoothly. So, 15000 km after installation, the second oil change time has come, so I decided to use this for the filter change this time.
This review is about item#40363565.
Oil management
4
From Japan
On 2017-09-30 15:58:17
We introduced it to three commercial vehicles. Difference came out when ranking 100 ~ 200 km with 2 out of 3 cars. It is a feeling that the low speed torque has risen. I am using 5w 40 oil. The models are Suzuki DA64V and HE22S.
This review is about item#40363592.
Regular oil change
4
From Japan
On 2017-09-14 18:09:17
It seems that engine rotation has become smooth though it is still several hundred kilometers after exchange. Since it is the first use, I am planning to change the next oil a little earlier.
This review is about item#40363565.
Maintenance of minicars
5
From Japan
On 2017-08-13 18:05:32
I do not want to teach it much, but it is a wonderful item! After exchanging oil (high-grade oil of monotaro) about 600 kilometers, the mass of sludge which had adhered to the large amount of the back side of the head cover got disappeared cleanly. Even if you trace with your fingers, it does not follow. I'm planning to replace dirty oil and use about 1000 kilometers. I think that price is reasonable, but thinking that it is cheap if you think about cleaning up by removing the engine. I do not go to replace expendable items like overhaul so I would like to clean it for the time being, I think that it is many times better than the additives of well-known manufacturers. By the way, it was impossible to say that the flushing oil of W company was so dirty as it got colored by pulling it off after idling for 30 minutes. Even though it is a good manufacturer for Dantotsu in the net reviews.
This review is about item#40363592.
Used for reducing sludge in the engine
5
From Japan
On 2016-09-29 16:19:24
After mounting 100 kilometers after installation, the engine rise improved. I will continue to use it.
This review is about item#40363592.
During oil change
4
From Japan
On 2015-07-15 15:01:27
Used for Honda Mobillio Spike Multi Car. Replace the element every second time when changing the oil and use this product. Although it used to replace the element three times already but it was originally used for a car with a slight rise of oil, it does not become a worse oil rise like afraid it is maintaining the present condition. For that reason it is unknown whether there really is such effect as written or not, but I feel that it is gradually getting better with engine sound stability and fuel consumption. Although it is a lot of long distance traveling, it is currently running at more than 16 Km, which was about 15 km before use. At the same time the oil itself is also changing, which effect is unknown. However, it is hard to buy it higher than oil price. If the price is half, I definitely want to continue using it but I'm having trouble.
This review is about item#40363565.
During oil change
4
From Japan
On 2014-11-15 01:11:41
I started running (installation) I ran 1,500 km, but it seems that it is about 3000 km replacement guideline but I feel that the engine system such as engine sounds became good. The product itself was like the main washing effect so I bought it I think that it was good.
This review is about item#40363592.
1
Customer Who Viewed This Item Also Viewed
Oil Filter Element
Oil Filter
Magnet Oil Filter
Magnet oil filter