Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of No.9400 W Sander T/C Long Sleeve Jumpsuit

No.9400 W Sander T/C Long Sleeve Jumpsuit
Sales Price: -
Review Rating: 4.17
6 Customer Reviews
5 star 3
4 star 1
3 star 2
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
For dirty work
5
From Japan
On 2015-11-20 14:46:32
Purchased because it is cheaper than buying working clothes at all. Material is not fluent, there is thickness as it is, so durability can be expected. Although it is a standard body type with a height of 170 cm, the length of the foot was quite long.
This review is about item#40390971.
Shipbuilding relations
4
From Japan
On 2015-10-27 09:52:28
The fabric is thin and right for the present time. It is the connection of the most standard type.
This review is about item#40390874.
Automotive electrical work
5
From Japan
On 2015-10-26 19:31:07
It seems that the pocket in which to put the ballpoint pen is slightly shallow. I want you to fall a little bit deeper.
This review is about item#40390856.
Vehicle electronics repair
3
From Japan
On 2015-08-20 21:29:22
Just for basic type this product. Very ordinary goods including fabrics. As usual for summer apple strength is wearing with confidence. When the fabric is 100% cotton, we are fearing short-term, shrinking, we are concerned about the strength of dilute sulfuric acid etc., we stick to synthetic fiber blend. Tsunagi clothes, I think that this very ordinary product is few in monotalou. Things that worry about the strength of the fabric, things with one side different from the pocket of the buttocks, things that do not know which country person's body was based on, one thing bigger than usual things that dig into another Yes. I think that it is a decent decade among them. I usually wear an L size. At first I ordered L, which is big like an idiot. Every time you lower your lower back, you can not lower your waist by putting up your thigh pads unless you raise the thigh fabric with both hands. I found that it was bigger than ordinary L size, so I thought that "M size should be large" and ordered M size. I usually can not wear M size, but I have not trouble wearing anything in the meantime. Just slightly smaller. I wanted a little more room. My height is 168 cm, weight 71 kg, and inseam 75 cm. I did not dig into the crotch even though I raised both hands while wearing an envelope. M size also applied Although the height was written as 165 cm, it is 3 to 5 cm in length by my height It is a state that the hem is too long. When taking off your shoes we fold 6 ~ 8 cm. And all the pockets want a little more depth.
This review is about item#40391066.
For installation work of computers etc
5
From Japan
On 2015-03-25 18:19:35
I am satisfied with good products with a good finish.
This review is about item#40390883.
Car maintenance
3
From Japan
On 2014-07-24 13:35:55
The product is normal. It took more than a month and a half between orders to arrive, even though shipment of item description is shown as 4 days. I contacted you on the inquiry form, but I did not reply. If you do not arrive, would you suggest to suggest alternative products or ask if you would like to cancel?
This review is about item#40390892.
1
Customer Who Viewed This Item Also Viewed
T/C Overalls
3120 Wata混 jumpsuit
Jumpsuit clothing 49112-2
(40230) pipe
Cotton Mix Boiler Suit
Jumpsuit clothes 49056