Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Hexagon Socket Head Screw UNS, Stainless Steel

Hexagon Socket Head Screw UNS, Stainless Steel
Sales Price: 4.99 SGD
Review Rating: 4.62
8 Customer Reviews
5 star 7
4 star 0
3 star 0
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 8 of 8 Reviews
Camera screw
5
From Japan
On 2018-02-28 15:54:07
Commonly known camera screw (U1 / 4) We used this product to replace the direct attachment head of the Velbon free camera head QHD - 63 to the Alcatswis clamp. Originally it was stopped with the M6 ​​screw from the inside of the ball but because Alkalam clamp is U1 / 4, I purchased it looking for this product of about the same length and thickness as the original screw but I am satisfied because it worked well I will.
This review is about item#41515381.
Screw change of motorcycle
5
From Japan
On 2017-09-03 22:17:51
It was hard to find nearby, and it was stem bolt I was looking for. It was saved.
This review is about item#41514934.
For US Astronomical Telescope
5
From Japan
On 2016-09-16 15:02:55
It is a unify screw which is difficult to obtain. It was able to be used without problems.
This review is about item#41515092.
work
5
From Japan
On 2016-03-16 13:42:28
Especially it is usable without problems.
This review is about item#41515783.
Fixing of large camera head for camera
5
From Japan
On 2015-06-05 14:44:04
Medium to large screw head mounting screws for cameras, so-called "thick screws" are this standard. Adapters that can be fixed in 1/4 "thin screws" in the female holes of thick screws are also on the market, but of course it is better to firmly fix them directly with thick screws.
This review is about item#41515695.
Used for Hurley's external goods clutch cover bolt
5
From Japan
On 2015-04-15 00:02:54
Although I inquired about dimensions, we were able to correspond quickly and politely and purchased the desired item. I am very satisfied and would like to ask in the future as well.
This review is about item#41515467.
Mounting of automobile parts
5
From Japan
On 2015-04-08 14:40:08
I was saved because it was hard to find the same size bolt.
This review is about item#41515564.
Fertilizer of the furnace
2
From Japan
On 2014-05-08 15:42:54
The goods are solid, but I did not notice at all until I ordered the wrong size and actually got the goods. Unlike familiar millimeter screws, the size is hard to understand so be careful when ordering next time.
This review is about item#41514234.
1