Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Insert Nut E Type, Iron, Trivalent White, Small Box

Insert Nut E Type, Iron, Trivalent White, Small Box
Sales Price: 32.99 SGD
Review Rating: 3.50
6 Customer Reviews
5 star 2
4 star 2
3 star 0
2 star 1
1 star 1
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
We used it for the assembly type furniture!
5
From Japan
On 2017-10-28 17:46:38
I used the same thing so far but this was cheap so I bought it all together! This ogre eye nut is most useful.
This review is about item#41845492.
Mounting the legs of the table
5
From Japan
On 2016-08-16 18:12:03
The unit price is cheap and the quality is also good. I will also purchase it.
This review is about item#41845501.
For knockdown
4
From Japan
On 2016-06-03 07:35:13
Is there a cheaper unit price a little more?
This review is about item#41845483.
Concluding timber
2
From Japan
On 2016-04-20 15:41:26
There is a thing in which the screw thread of M 6 part is crushed, and the screw does not enter. (1 piece at 24 points of use)
This review is about item#41845501.
Embed in wood, fasten the other parts. There is an advantage that you can choose the type of screw at that time.
1
From Japan
On 2016-03-02 20:28:30
Since when? The making became much stronger, the thickness of the main spindle changed. Notation of pilot hole is also displayed as 6 mm ~, but depending on wood, it is necessary to be more than 7 mm, so there are times when the dimension is severe so this specification change will be changed considerably on the design. There is a similar tendency in other size nibs, so you will need to try a trial before buying a box. After all, we have to look for and buy conventional standards at other shops.
This review is about item#41845474.
Fixing furniture
4
From Japan
On 2015-10-31 09:25:24
It will be saved when it becomes a little cheaper. It is easy to use item for fixing the furniture without problems for use.
This review is about item#41845535.
1