Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of (+) UNF (FLAT) Unified small screw (stainless steel)

(+) UNF (FLAT) Unified small screw (stainless steel)
Sales Price: 5.99 SGD
Review Rating: 2.00
1 Customer Reviews
5 star 0
4 star 0
3 star 0
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 1 of 1 Reviews
I want to bite the washer with the maintenance of imported equipment
From Japan
On 2017-04-16 18:41:07
I tried to purchase a 7/8-inch long threaded part with a length that I wanted to screw the washer to a US made screw of the equipment but I did not write it although I saw the measurement drawing. The first time I knew how to measure the length of the normal bolt (measure the length of the screw part without including the head) and this flat-head screw that the head enters (including not only the screw part but also the head) It was. Since it is a flat-head screw because it arrives, it can not be used in 7/8-inch including the head and it's not enough. All that is necessary is 7/8-inch screws so it is good if 1 inch flat-head screws are needed. Since it is impossible to return it, is not there anyway but would you please write down the measurement drawing of the screw firmly? Because it is an amateur, I do not notice the difference in how to measure the length of the screw easily.
This review is about item#41694947.