Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Flange Nut, Non Serrated, S45C H Chromate, Pack Product

Flange Nut, Non Serrated, S45C H Chromate, Pack Product
Sales Price: 4.99 SGD
Review Rating: 4.90
10 Customer Reviews
5 star 9
4 star 1
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 10 of 10 Reviews
Machine maintenance
5
From Japan
On 2018-02-06 15:49:34
The M8 nut is not sold to the home center and it is very handy
This review is about item#42108647.
During machine maintenance
5
From Japan
On 2018-01-29 19:06:07
There is no dissatisfaction about use and there is no trouble, I want to purchase
This review is about item#42108647.
Installation inside the control panel
5
From Japan
On 2018-01-23 14:55:12
There is no serrate of the flange nut in the home center so it is very helpful. It is good to be rust-resistant chromate. I want you to sell size 5 mm · 6 mm etc.
This review is about item#42108647.
Maintenance of motorcycles
5
From Japan
On 2017-09-27 20:30:34
I am glad that plenty of steel lineups are inexpensive.
This review is about item#42108647.
Used for attaching a muffler of a car.
5
From Japan
On 2017-09-26 04:03:31
It was not sold at the home center. I am satisfied with the performance. It's hard to say if you can choose a different type of plating.
This review is about item#42108647.
When car maintenance
4
From Japan
On 2017-09-21 00:44:43
Most of the flange nuts used for trucks (passenger cars in short) are without cerate. There are quite a lot of cases without cellate, but it seems that there are not too many, so the unit price feels pretty high. I think that it will become easier to use even a little cheaper.
This review is about item#42108647.
Replacement when motorcycle engine OH
5
From Japan
On 2017-08-07 19:59:25
M8 thanks to the sole choice of Giza-free flange nut, existence
This review is about item#42108647.
Motorcycle maintenance
5
From Japan
On 2017-03-04 12:35:13
Flange nuts used in automobiles and motorbikes are usually things that do not have cerate (jagged seating), but somehow the flange nuts sold at home centers etc. are only serrated. It is valuable that you can buy flanged nut without cerate in affordable pack items. However, even monoterror, the size such as 6 mm × P1.0 or 10 mm × P1.25 can be found only in an extreme number such as one thousand units. Since these sizes are often used in automobiles etc., demand is expected to be high, so we would like to sell small sellers. Also, I want you to sell small bag nut type.
This review is about item#42108647.
For motorcycles
5
From Japan
On 2014-04-07 06:47:32
A small dealer without cerate does not correspond with a neighboring home center or a dealer with a deal other than Monotaro so it is very helpful. However, since the price per plating of plating other than chromate is quite high, it will be saved if you get it to the same price as chromate.
This review is about item#42108647.
Vehicle maintenance
5
From Japan
On 2013-12-23 01:57:52
It is used for genuine part substitution of parts of two wheels, four wheels, power train where high torque is required. M8 size genuine products and strength no problem at all, can be used with specified torque. ☆ Recommended points · It is a high strength product of S45C. (Stainless steel is weak, caught at high temperature and high torque) · There is no serration (seating surface is not rough) · It uses durable chromate treatment on rust preventive surface. (Trivalent rusts immediately) ☆ Make sure that you can choose black zinc with different hue and different part of olive chromate treated product with higher rust prevention performance. · I want Mr. M6 size which is used frequently to be subdivided and sold in lineup. · I'd like you to align the screw pitch with the same size and detail. It is comprehensively a good product to think why people in the maintenance industry had never experienced it.
This review is about item#42108647.
1