Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Parallel Pin, Hard, Stainless Steel

Parallel Pin, Hard, Stainless Steel
Sales Price: 4.99 SGD
Review Rating: 4.00
8 Customer Reviews
5 star 4
4 star 2
3 star 1
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 8 of 8 Reviews
Movable shaft of plastic products
5
From Japan
On 2017-06-30 16:16:30
Although it is a small size, but the accuracy is good, even if you leave a gap, you can use it in the same way and it will be saved.
This review is about item#42204723.
As RC drive shaft pin
1
From Japan
On 2016-09-09 14:14:14
It is 1/10 buggy. I expected the phrase hard, but I ran away from 2 to 3 packs (less than 1 hour) with a battery, about 1/4 shaved. It will decrease to the form of D. After that, it is problem solving as pin of infinite precision machine. I wanted 10 mm, but it did not matter if it did not hit the surrounding even with 11.8 mm.
This review is about item#42205222.
Assembling parts
4
From Japan
On 2016-08-01 08:55:08
Where you can purchase in small lots is good, is not the fare cheap?
This review is about item#42205107.
Specifications fixed pin
3
From Japan
On 2015-09-26 13:16:43
It was able to be used without problems without problems or defects.
This review is about item#42205195.
Fabrication of screws
4
From Japan
On 2015-03-19 17:05:41
I would like to add items that are more soft and easy to process.
This review is about item#42205195.
Own product
5
From Japan
On 2014-11-14 15:32:01
The product accuracy is stable and good. We would like to reduce the cost by 100 units, 200 units.
This review is about item#42204906.
To the pin of the belt buckle.
5
From Japan
On 2014-04-24 16:35:24
Purchase of belt buckle pin, because it was missing and could not be found. Because it was between 2.0 mm and 1.6 mm in size, it was scraped off with metal file for metal and managed to fit in the hole. I bought it and was right. Thank you very much.
This review is about item#42205107.
I used it for the universal joint pin of a radio controlled car.
5
From Japan
On 2013-04-17 13:43:53
I used it for the universal joint pin, but I am very satisfied because it was inexpensive and precise. We have plenty of sizes and thinking of purchasing from your company when something happens.
This review is about item#42205116.
1