Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Stainless Steel Spacer Hexagonal/BSU(SUS303)

Stainless Steel Spacer Hexagonal/BSU(SUS303)
Sales Price: 4.99 SGD
Review Rating: 4.57
7 Customer Reviews
5 star 5
4 star 1
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
Extension of special shaft
5
From Japan
On 2018-02-16 00:26:24
It was very helpful since it is a product that I can not find easily. I will repeat.
This review is about item#42269595.
spacer
5
From Japan
On 2018-01-19 14:55:10
There are variations in length, so you can choose a good length just.
This review is about item#42269202.
As exterior parts of automobiles
5
From Japan
On 2018-01-05 08:44:59
It is made of stainless steel and seems to be durable. It was almost as image street.
This review is about item#42269604.
Production of test equipment
5
From Japan
On 2017-05-02 17:56:52
Combined with auxiliary kanag LK HK (Kameidadenki), we were able to produce the test equipment we wanted. There are various sizes, it is saved.
This review is about item#42269245.
Relocation of motorcycle equipment
4
From Japan
On 2017-03-06 07:50:49
Although the finish of the product is good, it is regrettable that the male screw is a bit longer than the entry size of the female screw.
This review is about item#42269604.
Grip fixing of bike handle and table creation
3
From Japan
On 2015-05-12 01:58:35
I bought a high thing but I bought L2 as short as 14 mm, it was not useful, 25 mm I searched but there is not anything cheap, I can not find it elsewhere.
This review is about item#42269647.
Changing takeout position of interfering lever
5
From Japan
On 2015-01-11 13:41:54
I screwed only the tip of a long M3 screw so far and fixed it with a nut, and fixed the lever with a double nut in the middle of the exposed screw, but when it changed to this spacer it became easy to install It was. Accuracy of screw thread was good, the perpendicularity of screw and long bolt part was satisfactory, and lever position could be changed neatly.
This review is about item#42269184.
1