Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Spoke Wrench

Spoke Wrench
Sales Price: 15.99 SGD
Review Rating: 4.25
4 Customer Reviews
5 star 2
4 star 1
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 4 of 4 Reviews
Bicycle maintenance
4
From Japan
On 2017-11-07 18:36:46
It is good to turn the nipples easily. It is good to see both ends for quick turning and high tension.
This review is about item#9293856.
To BMX
5
From Japan
On 2016-11-03 20:16:55
I can use it for BMX at all (nipple of odyssey) I think that it is hard to lick. However, it is hard to insert into the nipple a bit. It is bigger than I feel in the picture, it is sizing weakened by two thumbs.
This review is about item#9293856.
To the final finish of the spoke
3
From Japan
On 2015-11-16 08:49:29
Although I did not understand in the image, it was about 12 cm in total length and 83 g in weight, which was about twice what I was thinking. At the finishing stage of the aero spoke, the shape of the spanner shape is hard to get out, but when it was so large and heavy, I thought it was difficult for me to work.
This review is about item#09293856.
DT aluminum nipple turning
5
From Japan
On 2015-01-29 15:36:06
I use it when assembling the wheel with aluminum nipple of DT. There are two speech holes and it can be used for fast turning and high tension. It is cheaper than the park tool, but the accuracy is good.
This review is about item#43163976.
1
Customer Who Viewed This Item Also Viewed
Spoke Wrench
Nipple Wrench
Spoke SB Stainless
Combination Spoke Wrench
Spoke Wrench
Spoke Wrench
Spoke Wrench
Baided Spoke Holder
Spoke wrench
Spoke Wrench
Spoke nipple wrench
Spoke Wrench
Spoke Wrench
Spoke Wrench