Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Pipe Tap, PT

Pipe Tap, PT
Sales Price: 16.99 SGD
Review Rating: 3.80
5 Customer Reviews
5 star 2
4 star 1
3 star 1
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
Old thread mountain regeneration
From Japan
On 2017-09-19 15:48:13
It is enough in Cospa, because it does not cut the thread newly.
This review is about item#44546004.
I would like to use it to correct the screw of the pump
From Japan
On 2016-02-23 17:41:29
It is sufficiently helpful
This review is about item#44545986.
Thread cutting
From Japan
On 2014-07-16 07:56:16
I used it for processing the flange of the SS material. Because it was about 5 sheets, there was no problem with cutting. If there was a tap holder (socket wrench compatible type) that suits this, I bought it together, but that kind of thing did not seem to exist.
This review is about item#44545986.
Male screw processing.
From Japan
On 2014-04-13 10:59:29
BS and free-cutting aluminum (11S) can be used well.
This review is about item#44546004.
PT 3/4 size regeneration of crushed screw thread
From Japan
On 2013-11-13 19:39:04
Ideal for regenerating a crushed PT thread of an iron pipe. Also, I made a pilot hole of φ23.5 in ss400 and s25c and tried to make this PT3 / 4. Tool life is short. I challenged sus304, but my teeth did not stand at all. Therefore, it can not be used for sus304. Given the price, I think that it is better to use it for crushing screw mountain regeneration.
This review is about item#44546022.
Customer Who Viewed This Item Also Viewed
Pipe tap cone screw
Straight Thread Tap
Pipe tap
Parallel Thread Tap
Gastap (PT)
Tube Tap
Pipe tap (PS)
Pipe Tap PF
1/8 PT Pipe Tap
Tap for pipe
Taps for spiral tube
Gastap (PF)
Gas Tap