Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Chime AC Receiver Set

Chime AC Receiver Set
Sales Price: -
Review Rating: 4.00
7 Customer Reviews
5 star 1
4 star 5
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
Entrance chime
3
From Japan
On 2017-07-13 23:18:35
I thought that it was simple and easy to set, but when you set it to multiple outlet socket, the bottom outlet can not be used, so insert the bottom at the bottom I think that it is better to make it possible to use other outlets.
This review is about item#45495046.
Set up at the entrance. I am using it for signs at the time of visiting.
4
From Japan
On 2017-07-07 15:38:21
The wireless type is very easy to install and convenient. However, it is difficult for the transmitter to replace the batteries, but there is room for improvement. The back cover is difficult to open. Battery also 12V specification, it is also abandoning special.
This review is about item#45495046.
Call at meal
4
From Japan
On 2016-09-29 17:42:30
Since it does not have to be wired, it is extremely convenient to install anywhere. I think that it would be nice if there is something like "Rice is meal" or "I was able to eat" with a ring tone.
This review is about item#45495046.
Interphone
4
From Japan
On 2016-05-19 10:04:55
I appreciate easy installation. But as the other person wrote, what is the battery on the transmitter side, why just 5? Because it will be exhausted, it is about 3 A × 2.
This review is about item#45495046.
Outdoor installation
4
From Japan
On 2016-03-31 16:20:38
Monotaro says that the response was quick and courteous and relieved. It was able to be installed without problems and worked properly, the difficulty is that the volume is too large in two stages, it's too small, if there is stepless adjustment. It is hard to ask the transmitter battery. Well it is satisfactory.
This review is about item#45495046.
Call bell
5
From Japan
On 2015-11-04 22:08:26
Because it is AC on the receiving side, you do not have to change the battery so it will be GOOD
This review is about item#45495046.
Call from the store to the office
4
From Japan
On 2014-01-24 14:46:14
I think that it is good as a cheap calling chime with a clean design. The push comfort of the large button is also good. However, the ringing sound of the receiver has only switching of strength, strong is big enough to be surprised, sound is small for weak, I want a middle.
This review is about item#45495046.
1
Customer Who Viewed This Item Also Viewed
Chime, Sign Pet 100S
Call chime set
10ch call chime set
Wireless intercom
Wireless Chime Sensor Set
Wireless Chime Receiver
Wireless Chime Push Button
Chime Receiver