Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of NEW Anti Slip Tape SF

NEW Anti Slip Tape SF
Sales Price: 11.99 SGD
Review Rating: 3.75
8 Customer Reviews
5 star 4
4 star 2
3 star 0
2 star 0
1 star 2
The reviews are automatic translation.
Showing 1 - 8 of 8 Reviews
Internal staircase of the house
4
From Japan
On 2016-12-21 16:00:20
Adhesion is too weak! It will float immediately from the edge. The slip prevention effect is enough as it is regrettable.
This review is about item#45529897.
I purchased it to adopt it for slip prevention with a step difference, but adhesion was extremely weak and I decided to reject it,
1
From Japan
On 2016-11-29 21:20:21
I tried to stretch it with adhesive, but since it is soft, I am giving up because it is turned over, but I am giving up, I wonder if it will manage somehow, so that we can adopt it by devising how to use it when there is future of time I will give it a try, but for now it's getting in. I was disappointed. I would like you to make it even more powerful adhesive. I thought that it might be strong even if it is a hard material at the end, but as it is, it can not be used for our purpose. And it gets painful on the surface warts, so it's better to have a bit more soft Atari. It can not be disclosed under the content of this opinion. But since it is an honest opinion, I hope you do not feel bad. Because I am troublesome I will not do the return of the returned goods.
This review is about item#45529915.
Indoor door knob
1
From Japan
On 2016-11-13 23:13:02
Although there is no dissatisfaction with the shape etc., the adhesive tackiness on the back of the tape is very weak. Because the adhesion state is not so good, I use it with a strong double-sided tape in between, but there is a case that compatibility is not good with double-sided tape. Please improve it to be more sticky.
This review is about item#45529897.
Stair slip prevention
4
From Japan
On 2016-01-12 20:06:40
It is very easy to use and easy to work, but when riding with bare feet on the paste it seems a little painful but dimple is satisfactory in total.
This review is about item#45529915.
Used for the stairs.
5
From Japan
On 2015-11-08 08:29:00
It is a required item on the wooden stairs.
This review is about item#45529897.
Indoor staircase at home
5
From Japan
On 2013-11-19 13:39:16
I used it for an indoor staircase of about 12 steps, but the length and width were perfect, it was just right size I did not sell it to a home center etc and it was saved. With this I can rise and fall suddenly wooden stairs Thank you very much.
This review is about item#45529915.
Slip stop for stairs for playground equipment
5
From Japan
On 2013-09-11 13:14:13
The volume of 1 volume 5 m is less for use frequency, and most people use it. I want about 8 m or 10 m. The color is just right. Adhesion strength should be a little more.
This review is about item#45529915.
Slip on the entrance
5
From Japan
On 2013-06-18 14:30:51
It was just right size for a narrow step. It did not break the atmosphere of the entrance, it turned out a nice finish. I still have it, so I think what I should do. I was glad that it looks durable!
This review is about item#45529872.
1
Customer Who Viewed This Item Also Viewed
Anti Slip Tape
PYOLAN Non Slip Tape
Soft Anti Slip Tape
Anti-Slip Tape
Super Powerful Non-Slip Tape
Fluorescent Non-Slip Tape
Non Slip Tape
Non-Slip For Indoors