Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Digital Battery Level Checker

Digital Battery Level Checker
Sales Price: 21.99 SGD
Review Rating: 3.67
6 Customer Reviews
5 star 2
4 star 1
3 star 2
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
As a battery tester
3
From Japan
On 2016-11-23 03:53:08
I bought it to measure the remaining amount of batteries used at home. I think that it is good because it can be measured for each battery
This review is about item#46807871.
In order to measure the remaining amount of CR 123 A during periodic inspection
2
From Japan
On 2016-09-29 19:39:14
It is good that the battery used is a single 4 × 1. I would appreciate being able to measure the CR123A lithium battery. This is unexpectedly not supported. However, it seems that the setting that the residual quantity display comes out considerably more than the actual remaining capacity of the battery. For example, "I can use" → I can use it a little, "I can use it a little" → I can not use it. If you believe the result of this checker and measure the timing of battery replacement, you will mistake the battery replacement timing if you do not recognize that it is considerably less than the actual display. Apart from this model, it is the opinion of the results of measuring with a checker made by Sanwa Supply. For your information!
This review is about item#46807871.
Check battery level
5
From Japan
On 2016-03-29 21:11:25
Since the remaining amount is displayed exactly in the bar graph, it is very easy to understand, and it is pleasant even if you operate it. I should have bought it sooner.
This review is about item#46807871.
Battery check
3
From Japan
On 2016-03-17 22:37:30
As a simple checker to the last
This review is about item#46807871.
Battery level check
4
From Japan
On 2015-06-01 13:40:33
It is useful because it corresponds to 3V coin battery
This review is about item#46807871.
Check battery level
5
From Japan
On 2014-01-19 14:19:37
Until now, AA batteries etc. and button batteries were measured with separate checkers, but this digital battery remaining amount checker makes it convenient as it can measure all the batteries currently in use. I think that it will become compact once more by devising the back side if it speaks well.
This review is about item#46807871.
1
Customer Who Viewed This Item Also Viewed
Battery Checker
Rechargeable Battery Checker
Digital Battery Checker
Simple Battery Checker
Battery Checkers
Digital Battery Checker
Battery Tester
Digital Battery Tester
Mini Battery Checker
Multi Battery Checker
1.2V/1.5V Battery Checker
Glue Stick