Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Hose Clip SS

Hose Clip SS
Sales Price: 2.99 SGD
Review Rating: 4.80
5 Customer Reviews
5 star 4
4 star 1
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
Mounting of rubber & plastic hose
4
From Japan
On 2017-02-15 15:23:34
Speaking of quality, JCS's mild steel is better. But here is roughly half price! Army in here in Cospa. If it is a common thin plate band, it is hard to say that it is a uniform tightening because it sinks into the hose or the protrusion of the caulked part is large. Also tightening tightly makes it easy for the screw part to lick. In this type, the edge of the band is not pointed, and the protrusions of the caulked part are gentle so that it is firmly tightened. Even if it tightens strongly, it does not lick and it is safe. Points should be somewhat smaller size. Just fit enough to insert a little loose from the shipping state!
This review is about item#48861951.
When to tighten the hose
5
From Japan
On 2016-09-30 18:27:07
I bought other companies' roses with roses so far, but because I got to know this, the box selling is cheap and the product is well done so I will purchase other sizes from now on.
This review is about item#48862091.
To automobile radiator hose
5
From Japan
On 2016-06-15 16:27:52
Edge parts are processed smoothly, and quality of plating is very good so you can use it with confidence. Because prices are cheap, we use it in bulk purchase.
This review is about item#48861994.
Securing the blade hose
5
From Japan
On 2016-02-13 18:23:54
I entered a hose nipple with a blade hose 15 x 22 mm, outer diameter 14 mm, and it is stopped with this hose clip. It is hard to break and it stops securely so it is safe. Cost performance is high. Be careful as it may cause the blade hose to tear if it is tightened too strongly.
This review is about item#48861994.
Conclusion of Various Hoses for Automobiles
5
From Japan
On 2014-06-24 21:54:51
The hose band in the general home center has slits and irregularities on the inside but this product is excellent also in cospa because it does not bite into the hose with biting in the inside and it does not hurt the hose and it is not a single item but 10 pieces, So good!
This review is about item#48861994.
1
Customer Who Viewed This Item Also Viewed
Power Lock Band
Mini Clamp,SUS301
Hose Clips SUS
Nissan Type Clip
Disc Rotor
Steel Hose Clamp
JUBILEE Hose Clamp
Strong Machine Band A
(90466) Hose band
(47731) R piston
Fitting for blade hose