Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Wire Rope Slings

Wire Rope Slings
Sales Price: 4.99 SGD
Review Rating: 4.83
6 Customer Reviews
5 star 5
4 star 1
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
Opportunities used during maintenance
4
From Japan
On 2018-01-28 15:01:08
It was easy to use and the packaging was polite. I also want to use it.
This review is about item#48997347.
Panel in the exhibition
5
From Japan
On 2017-11-15 15:39:19
I bought without considering the thickness of the wire and hung the equipment side that needed somewhat small workmanship, but the hook side to hang on the panel hangs 3 kg product with no problems without problems.
This review is about item#58926393.
On the antenna pillar
5
From Japan
On 2017-07-13 21:17:30
Size, Thickness Various, purchased. It's a nice thing.
This review is about item#48997374.
For bike crime prevention
5
From Japan
On 2017-07-04 22:41:13
It is used in conjunction with a monoterroric dial lock to a fixed object.
This review is about item#58926384.
When leaving the scooter
5
From Japan
On 2016-12-06 17:41:39
I use a metal holder and a bag placed at my feet to prevent it from being stolen. It is good because it is coated with nylon.
This review is about item#48997347.
For helmet anti-theft
5
From Japan
On 2013-11-20 20:59:32
I bought it for helmet theft prevention. I use this through a large motorcycle to a Met holder. There is a length that can turn the helmet's jaw twice. Moreover, because the blue coating is done, scratch does not enter the object. Since it is possible to pass bags as well as helmets at the same time, it is convenient something if there is one. Cable in the anti-theft category is high for some reason.
This review is about item#58926384.
1
Customer Who Viewed This Item Also Viewed
Wire Rope
Wire Cut
W Sling A Type Wire
Satsuma Lock Slinging Wire
Out Stand Wire Winding Flemish
Socket 3H-19
Anchoring wire