Buy more than* S$200* and get FREE SHIPPING
Due to the maintenance, we will close our website on June/19 9:00-10:00 and June/23 0:00-0:30 JST. All customers cannot shop on our website during the time. Thank you.

Customer Reviews of Rainsuit

Rainsuit
Sales Price: 37.99 SGD
Review Rating: 4.42
19 Customer Reviews
5 star 12
4 star 4
3 star 2
2 star 1
1 star 0
The reviews are automatic translation.
Showing 1 - 19 of 19 Reviews
Construction work
5
From Japan
On 2018-04-28 14:56:03
Used at the construction site · It is not a work to do with an umbrella · It is very good because reflection is attached to the back.
This review is about item#333393.
When riding a motorcycle
5
From Japan
On 2017-11-25 01:36:45
The price is cheap and the making is solid. It seems to be pretty strong and long lasting.
This review is about item#00333393.
Bicycle commuting and light work
4
From Japan
On 2017-05-08 09:28:20
Until the rainy season, how far is the endurance life at this price in the blink of an eye?
This review is about item#333366.
Solar panel piping work
4
From Japan
On 2017-04-13 15:14:53
It is still 1 day to use, so it can not be said clearly, but I think that if you have durability it will be a safety shoe.
This review is about item#333375.
Used for motorcycle touring
5
From Japan
On 2017-04-03 22:17:29
I liked the color of turquoise and bought it. I like the visibility from other cars well.
This review is about item#333488.
Exterior wall cleaning of construction site etc.
5
From Japan
On 2017-03-16 12:40:51
I think that it is solid firmly because of the price. Although it will be weak while using it, I do not use it everyday, so I'm planning to buy it again after a year or two. Helmet is also useful because it covers.
This review is about item#333366.
Cleaning in factory
5
From Japan
On 2017-03-07 13:59:51
I tried it a lot so far and it cost so little that I did not last long because I did not last long, but I began to last long since I replaced it. very good.
This review is about item#333366.
Bicycle delivery on rainy day
5
From Japan
On 2016-10-24 13:36:36
Since it is not a moisture-permeable material, it is purchased for fall and winter. Be inexpensive. Purchasing motive is being PVC coated. Judging from the price I think that it will be acceptable if it can be used safely until the next rainy season.
This review is about item#333488.
On commuting
4
From Japan
On 2016-09-30 12:28:53
Even if I run by bike about 20 kilometers by commuting, it is GOOD that I have not tried it at all. However, because it is a pity that inundation from the zipper part is ☆ 4.
This review is about item#333506.
For motorcycle riding
3
From Japan
On 2016-07-12 19:44:07
Although it permeates, the inside does not stick to the body of the mesh. I am worried what happens if I wear it for a long time.
This review is about item#00333375.
Motorcycle commuting
5
From Japan
On 2016-06-12 18:55:07
It's easy to wear, and you can wear it comfortably.
This review is about item#00333375.
When working outdoors
5
From Japan
On 2016-03-17 15:28:29
I am satisfied that the making is firm regardless of the price. I refer to the size notation but I was slightly larger with a height of 178 cm, 3 L.
This review is about item#00333384.
For motorcycles
5
From Japan
On 2016-01-30 10:38:05
The reason for purchasing this product is that the lining is vinyl chloride coating rather than PU coating. If you use PU coating for a long time it will rain. The actual feeling of use is very good. The fabric is solid and free from rain leaks. There is no feeling of stiffness. The size is made slightly larger, but if you can afford to the pants of the pants when you cross the bike If there is only one order that is just right, I want you to increase the button to stop the waterproof fabric inside the outer jacket's chuck. I think that this idea is the opposite idea to ordinary rain gear.
This review is about item#00333375.
Driving a rainy motorcycle
5
From Japan
On 2015-10-08 20:07:21
There is no problem in quality at all. I will also purchase it.
This review is about item#00333488.
Motorcycle in the rain, driving a scooter
2
From Japan
On 2015-09-08 22:51:39
There is a mesh on the lining and it is comfortable even in the summer rain because it is not sticky. However, it is a little troubled that water comes into contact with tummy Atari.
This review is about item#00333488.
Motorcycle running
3
From Japan
On 2015-03-19 14:16:32
Especially the product itself is not complaining, but the color was not good. I think whether it is good if you can choose colors a little more.
This review is about item#00333497.
Motorcycle commuting
5
From Japan
On 2014-09-02 00:00:22
It is used for commuting at a scooter. I think that it is good, because it was firmly in price.
This review is about item#00333436.
Commuting
5
From Japan
On 2014-07-14 10:54:44
It is light and breathable and easy to wear.
This review is about item#00333375.
Motorcycle commuting
4
From Japan
On 2013-10-31 20:11:51
It is easy to move and comfortable is not bad.
This review is about item#52475701.
1
Customer Who Viewed This Item Also Viewed
Rainwear
Rainwear, Pegasus
Selection Rainsuit
Hybrid Rainsuit
B-10 Rain Suit
Rainwear, Takumi
Rising Mac
Defendered rain suit
Waterproof long coat
Planet Rain suit
Rain Wall Suit
Rain Suit