Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Soldering Station

Soldering Station
Sales Price: 239.90 SGD
Review Rating: 4.50
4 Customer Reviews
5 star 3
4 star 0
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 4 of 4 Reviews
When soldering the board
5
From Japan
On 2017-11-25 18:06:43
For soldering flat package IC etc. I am using it. There is enough calorie and the iron is light and easy to operate.
This review is about item#58072296.
Substrate soldering
5
From Japan
On 2016-04-06 14:47:31
It is affordable and easy to use. Since I was satisfied with the feeling of use after purchasing 1 unit, I bought two additional units.
This review is about item#58072296.
General soldering work at the factory
3
From Japan
On 2015-07-06 14:56:07
The temperature setting is digital and easy to understand
This review is about item#58072296.
Soldering
5
From Japan
On 2014-03-29 21:59:48
Although the frequency of soldering is not so high (1 to 2 hours per week on average), as "normal soldering iron" performs "while working", since the temperature rises excessively due to the heat of heat, I thought cleaning was troublesome. In that respect, "Station type soldering iron" has a solid temperature control so if you do not misunderstand the temperature setting you can proceed with your little tip in a very good condition. Since my friend used it since the Showa era, I knew the goodness of "station type" but the price became a bottleneck and did not come out. However, this product is not released with "hands-out price"! The check of new products in Showa head was sweet, I did not notice so we lost considerably. Well, this is a review of this product. Because the image of the conventional station was strong, I felt a sense of incongruity in appearance that "Iron Tab" and "Controller" were separated, but there are two types of "Iron Tabs" that are not heavy though they are not heavy The cleaner of the sponge is set, and the displacement prevention processing of the sponge cleaner is excellent in particular. This is an ant. "Temperature controller" which is set to 350 ° C by default is also wise. The time to get the practitioner temperature to the smallest tip is also very short, there is almost no waiting time. (In general soldering irons, when the temperature of the mini-hand exceeds 350 ° C, the coating falls and corrosion advances, so I often set it at 340 ° C.) The warranty period for a broken case is also very long So it is safe. I do not have such a tool to praise so much, but I do not see any faults. I can not bring myself to doing work without it.
This review is about item#58072296.
1