Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Air Chuck, Closed Type / No Hands Both Mouths

Air Chuck, Closed Type / No Hands Both Mouths
Sales Price: 32.99 SGD
Review Rating: 4.00
6 Customer Reviews
5 star 3
4 star 2
3 star 0
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
Used for replacing tires of large dump trucks
4
From Japan
On 2017-09-05 23:08:16
It is easy to use with a hands-free type, but I do not want durability of packing rubber and I often want to improve that I need to replace.
This review is about item#58162142.
When replacing truck tires
5
From Japan
On 2015-09-30 13:42:17
It is very convenient for letting go
This review is about item#58162167.
Tire inflation of light car
1
From Japan
On 2015-06-23 17:52:41
Whether it was incompatible with the valve, air is often leaked even if it is pressed. In addition, although manufacturers advertise that even if they release their hands by inner threads, they advertise that they are caught, but they are caught caught when they are pulled out. It is also not good to pull out the screw thread of the valve as if it scrapes off, as it will hurt the thread. For the above reasons I was not used as myself. Therefore, the evaluation is one star.
This review is about item#10711321.
I use it for my private truck
4
From Japan
On 2015-02-26 16:23:59
I am satisfied with this price because it is not used everyday.
This review is about item#58162142.
Tire inflation
5
From Japan
On 2014-11-18 17:41:36
OK
This review is about item#10711321.
Tire air refill
5
From Japan
On 2013-09-19 22:01:12
It was useful as it can be used for aluminum wheels of heavy-duty trucks.
This review is about item#58162185.
1
Customer Who Viewed This Item Also Viewed
Air Chuck
Air Chuck, Closed Type
Air Chuck, Closed Type / Couple
Air Chuck, ISO Method Wheel Support
Air Chuck, Open Type / Slim Couple
Super air chuck
Air Chuck, Closed Type
Air Chuck Gasket
Air Chuck
Air Chuck
Tire Chuck
Air Chuck Open
Air chuck (closed type / letting go lipped)
High-Spec Air Chuck