Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of AC adapter US series

AC adapter US series
Sales Price: 19.99 SGD
Review Rating: 4.83
6 Customer Reviews
5 star 5
4 star 1
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 6 of 6 Reviews
For powering LED lamp
5
From Japan
On 2018-01-09 14:59:26
It is small and ordinary good. I am glad that you can choose various specifications.
This review is about item#58392993.
As a substitute for the AC adapter of the wireless LAN router BUFFALO WHR-G301N
5
From Japan
On 2017-09-29 06:39:36
Wireless LAN router BUFFALO WHR-G301N POWER (green), DIAG (red) high speed lighting, does not work after turning on the power. Examination by the net is not the main body, the possibility of AC adapter breakdown is large. Purchased this product at 12V / 1A by being an EIAJ-4 AC adapter. It worked well.
This review is about item#58392993.
Used as a power source for the monitoring recorder of the entrance, the drive recorder became excessive when it wastefully scrapped.
4
From Japan
On 2017-03-29 11:29:08
I am using it somehow, but because the screen is small, it is not good
This review is about item#58393002.
Power supply for IC card reader / writer
5
From Japan
On 2017-02-07 19:59:40
The Panasonic JT - R200 CR - 10 non - contact IC card reader / writer AC adapter JT - 8000AD - 20 used in the store failed, 6 V 2 A connector shape EIAJ 2 is used as an alternative. At the card contracting company, it was estimate of more than 60,000 yen by exchanging a set of terminals, but for a while this seems to outperform.
This review is about item#58392975.
For charging handset
5
From Japan
On 2015-11-28 19:24:52
I can use it without any problem.
This review is about item#58393002.
For Logitech handlebar controller
5
From Japan
On 2014-02-09 22:49:47
It fits perfectly.
This review is about item#58393176.
1
Customer Who Viewed This Item Also Viewed
AC adapter UCB series
AC adapter UU series
AC adapter 20W
AC adapter 12W
AC POWER ADAPTER
AC Adapter UN Series
AC adapter UNL series
AC adapter UIA Series
AC Adapter UEA Series
DC9V Power Adapter
AC-DC adaptor 12V1A
AC adapter 24W
Ac Adaptor
AC Adaptor
AC Adapter