Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Snap Ring Pliers, Shank

Snap Ring Pliers, Shank
Sales Price: 22.99 SGD
Review Rating: 3.71
7 Customer Reviews
5 star 3
4 star 2
3 star 0
2 star 1
1 star 1
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
Removing the snap ring of the racing cart engine
1
From Japan
On 2017-08-10 21:30:01
The rigidity of the tip was very weak, and the tip bent with the detachment of two snap rings. It was the worst tool among the items I bought with Monotaro.
This review is about item#8382367.
Maintenance of old general-purpose lathes. Exchange of snap ring in narrow gearbox space
5
From Japan
On 2016-12-01 01:25:45
In other companies' products, the handle was too big to work in a narrow space. It was a bit small, so it was just fine. It was also easy to use because the snap ring was caught securely. Until now, in the gearbox, since the handle touched the gear and the snap ring of the pulley shaft in the back could not be exchanged, it was really saved.
This review is about item#08382394.
Repair of milling cutter
4
From Japan
On 2016-10-29 16:46:59
As I got lost again on business trip, I arrived early and it was saved.
This review is about item#8382367.
Mission assembly
5
From Japan
On 2015-10-14 15:55:39
It is easy to use familiarly with the clip to use.
This review is about item#08382464.
Bearing exchange
2
From Japan
On 2015-03-18 16:25:44
My mouth is too wide. Even if the shaft diameter is matched, the hole pitch has not been matched since the mouth is open.
This review is about item#08382367.
When the engine is disassembled
5
From Japan
On 2014-10-16 16:52:44
There is rigidity not to be defeated by the tension of the snap ring, so workability is very good.
This review is about item#08382385.
For plug detaching
4
From Japan
On 2013-03-20 23:18:32
Because it has a stopper, it is very easy to use. The degree of parallelism of the tip is now one more thing.
This review is about item#08382473.
1