Buy more than* S$200* and get FREE SHIPPING
Due to the maintenance, we will close our website on June/19 9:00-10:00 and June/23 0:00-0:30 JST. All customers cannot shop on our website during the time. Thank you.

Customer Reviews of Net, Stainless Steel Plain Woven Wire Mesh

Net, Stainless Steel Plain Woven Wire Mesh
Sales Price: 36.99 SGD
Review Rating: 4.17
12 Customer Reviews
5 star 4
4 star 6
3 star 2
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 12 of 12 Reviews
Prevention of pest infestation
5
From Japan
On 2018-05-03 15:43:27
Since the bee invades from the vent hole of the wall and makes a nest in the attic, it cut it into the size of the frame from the back of the ventilation opening and constructed it. I easily cut it with scissors so it was easy to process.
This review is about item#60847376.
Prevention of clogging of snow at suction opening of outdoor unit
4
From Japan
On 2018-02-10 16:29:39
I wanted a size of about 1.5 m instead of 1 m. The size is insufficient for large air conditioners.
This review is about item#60847394.
Paper utensils
4
From Japan
On 2017-11-26 01:35:31
Quality is good. Specification as a tool for paper making. I use it in a water field, but it does not rust. It is good that the price is cheaper a little, but it is saved because there is no neighborhood home center.
This review is about item#60847385.
For ventilator insect repellent
3
From Japan
On 2017-11-22 15:02:19
Items have been sent in rolled form. Because the thickness was small, making a habit was difficult. I think that it is good to round off a little slowly.
This review is about item#60847351.
Cutting fluid filter
5
From Japan
On 2017-03-03 16:06:34
I am using it to remove the facet with mesh No. 40. If it is only number 40, a fine facet will pass. It seems that almost 100 can be removed if it is added to 2 stages.
This review is about item#60847385.
Backing of underfloor vent
4
From Japan
On 2017-02-27 08:15:34
I was glad that the shape was firmer than I thought. Many types were selected.
This review is about item#60847351.
Used for air intake, rough eyes are available locally but there is no net of squirrel.
5
From Japan
On 2016-08-23 19:55:29
Easy to process, we are going to add an order as soon as it gets lost at reasonable and cheap price.
This review is about item#60847385.
Sand shaking
5
From Japan
On 2016-05-08 18:24:10
I was glad that I could shake the size suitable for my job.
This review is about item#60847385.
Measures to prevent invasion of insects from the vent hole of the foundation
4
From Japan
On 2015-08-27 16:19:02
With universal scissors according to the size of the vent hole, cut it, hammered with a horn with a piece of square piece, did not get used to the casting lattice of the previous customer, and fixed with a denatured silicone adhesive. Half of the material is sufficient for five measures. If you add to the display data of the product what is the decline in ventilation efficiency, it will contribute to appropriate judgment in various application situations. The target of this measure was Kamadoma.
This review is about item#60847351.
Outdoor
4
From Japan
On 2015-04-05 21:48:44
Heat resistant and lightweight, so purchase for use on fireflies. As you like, I thought it was a bit more soft, so I purchased 0.14 mm at the same time.
This review is about item#60847367.
Insect control
3
From Japan
On 2014-08-16 23:51:37
Thinking in terms of size, it was quite expensive.
This review is about item#60847351.
Used as a protection for indoor lighting lamp of sandblasting machine
4
From Japan
On 2014-08-12 13:44:30
It is used as a protection of the lighting lamp inside the harsh sandblasting machine. Although it is helpful for protection enough, I think that it would be better to extend the life of the net a little more.
This review is about item#60847385.
1
Customer Who Viewed This Item Also Viewed
Net, Stainless Steel
Stainless Steel Wire Net
Vinyl Mesh Netting
Galvanized Mesh Netting
Stainless Steel Mesh Roll
Aluminum Mesh Netting
Mesh Netting
Back net
Do-it-yourself wire mesh
Mesh-Rack Side Net