Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of General Purpose Pressure Gauge

General Purpose Pressure Gauge
Sales Price: 15.99 SGD
Review Rating: 5.00
5 Customer Reviews
5 star 5
4 star 0
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
For checking the pressure of air piping
From Japan
On 2017-09-11 15:49:02
I purchased and used several MonotaRO's pressure gauges on the piping which normally takes about 0.69 to 0.78 MPa, but the indicated value becomes strange in about one year, and as soon as I examine the pressure, the pointer returns to 0 It was gone. I would like to replace it with this product in the future. I do not know how durable it is yet, I made it to 1.6 MPa full scale, so I do not think it will be broken soon.
This review is about item#60996661.
For air compressor piping pressure reducing valve adjustment
From Japan
On 2017-08-16 02:52:45
It is cheap but necessary and sufficient. I use it without any problem. Durability is not understood yet.
This review is about item#60996661.
For aquarium oxygen
From Japan
On 2017-06-13 21:27:39
Although it was able to be used enough, it was too expensive, but it was good value, so it was good.
This review is about item#60996591.
Air Compressor
From Japan
On 2016-02-29 15:54:20
Since the gauge of the compressor was broken, I used it for replacement. You can use it enough.
This review is about item#60996661.
Compressor pressure gauge exchange
From Japan
On 2014-11-28 23:58:48
Three-phase 200V reciprocating compressor pressure gauge broke down, so purchased for replacement. Those of other manufacturers were attached as genuine, but choose a low price here. Although the parallel thread specification was even cheaper, I made it to the tapered screw specification according to the original one. Making is also firm with respect to price and measures accurately. Cost performance is good.
This review is about item#60996677.
Customer Who Viewed This Item Also Viewed
Pressure Gauge
Pressure Gauge, Ф60
Pressure Gauge Type A phi75
General-Purpose Manometer
Pressure Guage
Pressure Gauge, All Purpose
Small Pressure Gauge
Pressure Gauge, Drip Proof, Ф75
Pressure Gauge, Drip Proof, Ф60
Small Pressure Gauge A form Vertical phi40
Small Pressure Gauge (Vertical-collarless)
Small Pressure Gauge A form Vertical phi50
Vibration-proof Pressure Gauge
Pressure Gauge