Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Pop Nut

Pop Nut
Sales Price: 5.99 SGD
Review Rating: 4.80
5 Customer Reviews
5 star 4
4 star 1
3 star 0
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
Connection of bolt
5
From Japan
On 2018-01-19 17:19:50
Since the screw is stopped at the center part, it stops just at the center when screwing in from both, so it is easy to squeeze. I think that there is something about 20 mm through which the rear female thread penetrates. I cut it with only one 20 mm available.
This review is about item#88143763.
Bolt connection in hollow pipe
5
From Japan
On 2017-07-02 15:10:31
It was used to extend a special bolt inside a hollow pipe. I think that it is even better if it sells even the size of the fine thread.
This review is about item#88143867.
Motorcycle turn signal stay extension
4
From Japan
On 2017-01-15 15:53:23
Since the turn signal was hidden when the bikini cowl was attached to the bike, I wanted M10 x 50 mm P 1, 5 for purchase for extension. I bought it with a bet without the notation of screw pitch. Although dispatch was early, arrival was quite late · · At this time Kobe - Kanagawa is not possible to lose 4 days?
This review is about item#88143815.
ULP shaft of ULP machine
5
From Japan
On 2016-06-16 21:29:47
The finish is beautiful, lightweight, you can choose it with abundant size
This review is about item#88143833.
Car shift knob extension
5
From Japan
On 2016-05-28 18:18:05
It was too long for the regulated goods, so I bought it. I am perfect fit, thank you.
This review is about item#88143763.
1
Customer Who Viewed This Item Also Viewed
Round Spacer, SUS303
Round supporter
Stainless Round Nuts
Steel Round Nuts
Long Hexagon Nut
EYE BOLTS
Iron Round Boss
Tapped Tube, Iron, Pack Product