Buy more than* S$200* and get FREE SHIPPING
Due to the national holidays as Golden Week, we will close 2018/4/28~2018/4/30 and 2018/5/3~2018/5/6.
This may cause delays with our responses. Thank you for your understanding.

Customer Reviews of Long Reach T Handle Wrench

Long Reach T Handle Wrench
Sales Price: 11.99 SGD
Review Rating: 3.57
7 Customer Reviews
5 star 2
4 star 2
3 star 2
2 star 0
1 star 1
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
Motorcycle maintenance
3
From Japan
On 2017-03-26 16:11:17
Because satin finish processing is rough, I feel caught in a glove glove. I rubbed the surface lightly with paper and it became moderately rough. It is a thoroughly satisfying thing if you choose by focusing on COSPA because you can not see the top.
This review is about item#75263072.
Motorcycle repair
4
From Japan
On 2017-01-30 22:44:18
I bought a head angle of 10 mm. It is OK even if the handle part is a little short, and the longer the wrench length, the more useful it is. Because it is low cost, I can use it without hesitation.
This review is about item#75263081.
Motorcycle maintenance
5
From Japan
On 2015-10-16 19:54:08
Accuracy is good without licking.
This review is about item#75263081.
Auto Repair Service
1
From Japan
On 2015-05-02 18:56:57
It was garbage.
This review is about item#75263072.
Work in narrow and deep place.
4
From Japan
On 2014-12-03 14:25:58
T type wrench, if you can replace the socket is the best! 6.3 mm or 9.5 mm socket available T type wrench.
This review is about item#75263072.
Used for scooter oil change
5
From Japan
On 2014-05-07 20:09:12
I bought it because the drain bolt of YAMAHA's 50cc scooter was 12mm and I wanted a long wrench for my neck. Easy to use and convenient.
This review is about item#75263097.
Motorcycle maintenance
3
From Japan
On 2014-05-01 15:10:02
T type wrench has not used much, so purchase what kind. In normal use there is no problem first. But it is 6 points, it is not a face contact, the wall thickness is not as thin as a famous manufacturer's socket wrench, and the shaft is satin finish so it feels like when it is fast turning · · · There is a margin for money If you are looking for quality, I think that it was better for you to ask for the mirror finished goods of famous manufacturers obediently.
This review is about item#75263072.
1
Customer Who Viewed This Item Also Viewed
TB T Type Box Wrench
BB T Type Square Box Wrench
T form wrench
T-shaped wrench short handle
T Handle Wrench
T Handle Wrench
T-type wrench
T-Handle
Fast Turn T Form Wrench
Wrench 14X15MM
T-shaped handle 3 minutes 300
T-handle 4 minutes 300
T-Handle
T-shaped Mission handle 654mm
T-shaped Mission handle 650mm
T-long box wrench
T-type wrench