Buy more than* S$200* and get FREE SHIPPING

Customer Reviews of Welding Mask

Welding Mask
Sales Price: 60.99 SGD
Review Rating: 4.40
5 Customer Reviews
5 star 3
4 star 1
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 5 of 5 Reviews
When TIG welding
3
From Japan
On 2018-02-07 09:31:19
Although it is solidly made for the amount of money, I think whether the spring of the window is too strong.
This review is about item#75900307.
Arc welding
5
From Japan
On 2017-10-21 21:45:59
As of now it is the most user friendly. The position at the time of shaking it down is stable. It is convenient when there is flip when dropping slag.
This review is about item#75900307.
For tig welding
5
From Japan
On 2016-09-27 19:59:19
When purchasing only the face for the first time for automatic liquid crystal, unexpectedly undoing the flip unexpectedly made a dent of 50 × 110 mm, the headgear was broken and the large size liquid crystal that was left was fitted. Since there is thickness, I could manage to improve the spring with pliers etc. Somehow, I was able to use it just like exchange side. Since it is irregular, I am worried about whether it is good to post, but, as a thing, I feel that the balance of weight etc. is firmly made well.
This review is about item#75900307.
welding
4
From Japan
On 2015-10-22 11:02:52
It was quite easy to use.
This review is about item#75900307.
Used for TIG welding with auto light shield plate attached
5
From Japan
On 2015-07-02 21:00:00
Even if you raise it up, it does not fall and it does not go too far down, so it is pretty solid. I have been using expensive items until now but this is enough for me.
This review is about item#75900307.
1
Customer Who Viewed This Item Also Viewed
Welding Face Shield
Welding Helmet, LCD
Welding Face Shield
Welding Shield Glass
Welding Mask
Welding Shield Glass
Welding Cover Plate
Welding Shield Glass
Welding Shield Glass