Buy more than* S$200* and get FREE SHIPPING
Due to the maintenance, we will close our website on June/19 9:00-10:00 and June/23 0:00-0:30 JST. All customers cannot shop on our website during the time. Thank you.

Customer Reviews of Small Vises

Small Vises
Sales Price: 27.99 SGD
Review Rating: 4.50
8 Customer Reviews
5 star 5
4 star 2
3 star 1
2 star 0
1 star 0
The reviews are automatic translation.
Showing 1 - 8 of 8 Reviews
Small, fixation of parts when soldering pin connector
4
From Japan
On 2018-03-03 23:30:11
The size is reasonable and very good. However, the place of holding was a bit poor and unstable. Sometimes it is not possible to secure firmly. However, if it is this price, it can be convinced
This review is about item#86923462.
It is used for fixation when machining small parts of plaque and fixing for microscopic photography with digital camera.
5
From Japan
On 2017-11-28 16:26:45
Since it is compact, it can be used without worrying even in a narrow space, so it is very useful. Improvement point is that when chucking an object, fixing it to the end of the mouth, the mouthpiece is inclined and a coarse phenomenon occurs at the time of tightening.
This review is about item#86923453.
Modify it to make it easy to use
5
From Japan
On 2017-08-28 10:02:46
There is a good item because it is heavy at this size. There is a backlash in the mouthpiece and it is hard to fix, but I am using it for reconstruction. It is due to the thin shaft that goes through the mouthpiece. Replacing the shaft to 2.4 mm or 2.5 mm makes it easy to use. There are 3 units, but all of this is remodeling in this way. Sometimes the middle of the bottom plate is not flat, but it also makes it flat with a sandpaper.
For fixing part during part molding
3
From Japan
On 2016-12-22 23:39:05
It is good to work with weight being moderate by hand, but there is more rattling than I thought, it is somewhat difficult to fix small parts. Is it such a thing from the price?
This review is about item#86923453.
Work of model etc.
4
From Japan
On 2016-09-29 18:07:26
Although it is good as a vise, it stopped with the split pin for preventing the screws of the operating part from coming off, but it came straight out and the screws came out of the way back. I cut off the tap of M5 and fixed measures with an emonji screw. The manufacturer should take measures!
This review is about item#86923462.
Fine work
5
From Japan
On 2016-06-24 16:29:45
I use it as a substitute for a hand that supports during soldering such as a plug. Bakedo has become less. It is also used when cutting small pipes. It is small but it has a solid feeling.
This review is about item#86923453.
For fixing the fuselage of the wing and tail wing of the Balsa airplane at the time of adhesion
5
From Japan
On 2015-11-10 02:35:17
It is small, but it is securely fixed and very convenient
This review is about item#86923462.
Used for soldering on desktop
5
From Japan
On 2014-12-19 13:12:16
It is good to use it, but it will be better if the magnet fixing is possible!
This review is about item#86923453.
1
Customer Who Viewed This Item Also Viewed
Vise
  • Vise
  • HOZAN TOOL INDUSTRIAL CO.,LTD.
  • 37.99 SGD
  • 3.000000(2)
Yankee Vice
Drill press vise
Alumi vise
Yankee Vice
Yankee Vice
Vise
  • Vise
  • HOZAN TOOL INDUSTRIAL CO.,LTD.
  • 59.99 SGD
Machine Vise
Aluminum Quick Vise
Precision vice
Mini Vise
Vise
Precision vice
Precision Minibaisu