Buy more than* S$200* and get FREE SHIPPING
Due to the national holidays as Golden Week, we will close 2018/4/28~2018/4/30 and 2018/5/3~2018/5/6.
This may cause delays with our responses. Thank you for your understanding.

Customer Reviews of Chamfer Cutter

Chamfer Cutter
Sales Price: 15.99 SGD
Review Rating: 3.71
7 Customer Reviews
5 star 3
4 star 2
3 star 0
2 star 1
1 star 1
The reviews are automatic translation.
Showing 1 - 7 of 7 Reviews
Deburring M3 tapped hole
2
From Japan
On 2018-02-18 14:05:05
I bought it for burr removal of the M3 tapped hole, but the blades do not mesh well. A little more sharp type or smaller diameter seemed better.
This review is about item#86925176.
Machine maintenance
4
From Japan
On 2017-06-21 11:00:41
I used it for dish of M8 flat head screws, but it is a bit small. I want another 0.5 mm. Sharpness is good.
This review is about item#86925194.
When metal working.
5
From Japan
On 2017-04-21 17:04:35
It is convenient to use for woodworking as well as metal processing. Good durability performance.
This review is about item#86925185.
Deburring holes etc.
4
From Japan
On 2017-02-09 23:35:12
As we used the chamfering cutter in the drilling machine, we replaced it, so we replaced it. Vibrations rarely occur, if deburring it can be used even if you turn by hand if the other is aluminum.
This review is about item#86925176.
It is also processed into brass 3, 5 mm holes.
1
From Japan
On 2017-01-12 21:46:35
I attached it to the drilling machine and processed it but the blade did not cut at all and I could not process any one. Is the purpose different?
This review is about item#86925176.
Dish wood screws for sinking heads for chamfering
5
From Japan
On 2016-04-25 22:58:11
I used MC - 12 for hand drill, but purchased MC - 8 for tabletop drilling machine. It is sufficient ability for woodworking.
This review is about item#86925176.
For chamfering for countersunk screw holes
5
From Japan
On 2015-10-26 18:13:58
I was looking for a chamfering cutter to make a countersink of 2 mm countersunk screw into a 1 mm thick FRP plate. I could not find a nice tool very well because the countersunk hole I want to open is small, but it was able to be processed perfectly with this cutter. If you are an FRP partner, you can process it satisfactorily by grabbing it directly by hand without attaching it to a drill etc, but if you want accuracy, it is recommended to be mounted on a drilling machine etc. I'm glad that the price is cheaper a bit, but I am satisfied because it seems that FRP partners will be able to use it once they buy it once.
This review is about item#86925176.
1
Customer Who Viewed This Item Also Viewed
Chamfering cutter
Counter sink
Center Reamer 90deg
Center Reamer 60deg
Countersink 60 Degree
Counter sink
Hex Shank, Nice Men
Chamffering Cutter
Counter sink
Mentorikatta
  • Mentorikatta
  • Mitsubishi Hitachi Tool Engineering (former Hitachi Tool Engineering)
  • 16.99 SGD
  • 4.750000(4)
Center reamer 120